Skip to main content
aziubin
Graduate
November 29, 2023
Solved

Multiple STHS34PF80 IR sensors nearby each other.

  • November 29, 2023
  • 1 reply
  • 1586 views

Can several STHS34PF80 IR sensors be used simultaneously, when placed not far from each other, say on the same PCB? If STHS34PF80 infrared sensors are completely passive devices, there should not be any limitations of the distance between them, even if their fields of view are intersecting, right?

 

This topic has been closed for replies.
Best answer by Peter BENSCH

Correct, the STHS34PF80 are purely passive components and can be positioned directly next to each other without any problems and without any mutual interference.

Good luck!
/Peter

1 reply

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
November 29, 2023

Correct, the STHS34PF80 are purely passive components and can be positioned directly next to each other without any problems and without any mutual interference.

Good luck!
/Peter