Skip to main content
Associate III
September 22, 2025
Solved

ODR_XL[3:0] operation of ASM330LHH

  • September 22, 2025
  • 1 reply
  • 364 views

We sincerely appreciate your continued support. We have been able to resolve many questions.
In the CTRL1_XL register of the ASM330LHH, when setting ODR_XL[3:0] from 0000 (OFF) to 0011 (52Hz) and then to 1001 (3333Hz), does ODR_XL[3:0] need to be set back to 0000 (OFF) once ?

Best answer by Federica Bossi

Hi @ggob ,

No, it is not necessary.

1 reply

Federica Bossi
Federica BossiBest answer
Technical Moderator
September 22, 2025

Hi @ggob ,

No, it is not necessary.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.