Skip to main content
Associate III
September 2, 2025
Solved

Order of operation of INT2_CTRL (0Eh) in ASM330LHH

  • September 2, 2025
  • 1 reply
  • 154 views

Should INT2_CTRL (0Eh) in ASM330LHH be changed when ODR_XL[3:0] in CTRL1_XL is 0, or should it be changed after being set to non-zero?

Best answer by Federica Bossi

Hi @ggob ,

It is recommended to configure INT2_CTRL only after enabling the accelerometer with a non-zero ODR.

 

1 reply

Federica Bossi
Federica BossiBest answer
Technical Moderator
September 11, 2025

Hi @ggob ,

It is recommended to configure INT2_CTRL only after enabling the accelerometer with a non-zero ODR.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.