Skip to main content
VPrad.2
Visitor II
September 23, 2024
Question

Pedometer in lsm6dsox not working

  • September 23, 2024
  • 1 reply
  • 741 views

Hi all,

About 25% of the LSM6DSOX sensors in the field have a non-functional pedometer. The step count is showing as zero. A power-on reset or software reset does not resolve the issue. We rely on the step count provided by the pedometer module, but it is consistently reading zero. The wake-up interrupt is working correctly, but the step count interrupt and direct reading from the step count register both return zero. Please assist in addressing this issue. This is very critical as we are replacing a lot of devices because of this.

 

Thanks,

Vishnu Pradeep

1 reply

Federica Bossi
Technical Moderator
September 25, 2024

Hi @VPrad.2 ,

That sounds very strange. Did you follow our official PID example?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.