Skip to main content
Associate
March 17, 2025
Question

Problem with Heading Calculation

  • March 17, 2025
  • 1 reply
  • 439 views

I'm using ST MotionFX v2.7.1 and have encountered an issue with heading calculation.

I'm following the sample code from the document:
um2220-getting-started-with-motionfx-sensor-fusion-library-in-xcubemems1-expansion-for-stm32cube-stmicroelectronics

 

#define STATE_SIZE (size_t)(2450)
static uint8_t mfxstate[STATE_SIZE];
MFX_knobs_t iKnobs;
MFX_input_t data_in_scale;

void main() {
 /* Sensor Fusion API initialization function */
 MotionFX_initialize((MFXState_t *)mfxstate);

 /* Modify knobs settings & set the knobs */
 MotionFX_getKnobs((MFXState_t *)mfxstate, &iKnobs);

 iKnobs.LMode = 2;
 iKnobs.modx = 1;
 iKnobs.output_type = 1;
 iKnobs.start_automatic_gbias_calculation = 1;
 
 //orientation

 MotionFX_setKnobs((MFXState_t *)mfxstate, &iKnobs);

 MotionFX_enable_6X((MFXState_t *)mfxstate, MFX_ENGINE_DISABLE);
 MotionFX_enable_9X((MFXState_t *)mfxstate, MFX_ENGINE_DISABLE);

 /* Enable 9-axis sensor fusion */
 MotionFX_enable_9X((MFXState_t *)mfxstate, MFX_ENGINE_ENABLE);

 // init last_time
 clock_gettime(CLOCK_MONOTONIC, &last_time);

 get_sensor_data_scale(&data_in_scale);

 MFX_input_t sensor_in;
 MFX_output_t sensor_out;

 for(int i =0; i< 9999999999; i++)
 {
 get_sensor_data(&sensor_in);

 float delta_time = get_delta_time();
 MotionFX_propagate((MFXState_t *)mfxstate, &sensor_out, &sensor_in, &delta_time);
 MotionFX_update((MFXState_t *)mfxstate, &sensor_out, &sensor_in, &delta_time, NULL);

 printf("Heading: %f\n", sensor_out.heading);
 }
}

 

 

When I run the code, the heading value is incorrect. However, if I re-run MotionFX_initialize, the heading calculation becomes correct.

 

#define STATE_SIZE (size_t)(2450)
static uint8_t mfxstate[STATE_SIZE];
MFX_knobs_t iKnobs;
MFX_input_t data_in_scale;

void main() {
 for(int i =0; i< 9999999999; i++)
 {
 /* Sensor Fusion API initialization function */
 MotionFX_initialize((MFXState_t *)mfxstate);

 /* Modify knobs settings & set the knobs */
 MotionFX_getKnobs((MFXState_t *)mfxstate, &iKnobs);

 iKnobs.LMode = 2;
 iKnobs.modx = 1;
 iKnobs.output_type = 1;
 iKnobs.start_automatic_gbias_calculation = 1;

 //orientation

 MotionFX_setKnobs((MFXState_t *)mfxstate, &iKnobs);

 MotionFX_enable_6X((MFXState_t *)mfxstate, MFX_ENGINE_DISABLE);
 MotionFX_enable_9X((MFXState_t *)mfxstate, MFX_ENGINE_DISABLE);

 /* Enable 9-axis sensor fusion */
 MotionFX_enable_9X((MFXState_t *)mfxstate, MFX_ENGINE_ENABLE);

 // init last_time
 clock_gettime(CLOCK_MONOTONIC, &last_time);

 get_sensor_data_scale(&data_in_scale);

 MFX_input_t sensor_in;
 MFX_output_t sensor_out;

 get_sensor_data(&sensor_in);

 float delta_time = get_delta_time();
 MotionFX_propagate((MFXState_t *)mfxstate, &sensor_out, &sensor_in, &delta_time);
 MotionFX_update((MFXState_t *)mfxstate, &sensor_out, &sensor_in, &delta_time, NULL);

 printf("Heading: %f\n", sensor_out.heading);
 }
}

 

 

Does anyone know why this happens? Any insights would be greatly appreciated! Let me know if you need more details.

1 reply

Federica Bossi
Technical Moderator
March 21, 2025

Hi @gtk ,

Can you share the outputs you get in both cases?

Thanks!

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
gtkAuthor
Associate
March 25, 2025
//without 9x

mag: [-0.208000, -0.996000, 0.565000]
acc: [9.514451, 1.042671, 0.016750]
gyro: [0.009163, -0.059559, 0.056047]
Yaw: 350.114685, Pitch: -0.101226, Roll: 6.254028
Quaternion: [W=0.005579, X=-0.054271, Y=0.086079, Z=0.994794]
Gravity: [X=-0.108937, Y=-0.001756, Z=-0.994047]
Linear Acceleration: [X=0.933735, Y=0.014994, Z=8.520404]
Heading: 350.114685
Heading Error: 0.417009
==============================
mag: [-0.214000, 0.873000, 0.604000]
acc: [9.762706, 1.114456, -0.442074]
gyro: [-0.070555, -0.111177, 0.226325]
Yaw: 350.849396, Pitch: 2.392230, Roll: 6.477042
Quaternion: [W=-0.016269, X=-0.057963, Y=0.078449, Z=0.995099]
Gravity: [X=-0.112805, Y=0.041474, Z=-0.992751]
Linear Acceleration: [X=1.001651, Y=-0.400600, Z=8.769955]
Heading: 350.849396
Heading Error: 0.300941
==============================
mag: [-0.214000, 0.858000, 0.616000]
acc: [9.881749, 0.461216, -0.324825]
gyro: [-0.071166, -0.021686, -0.625525]
Yaw: 5.967731, Pitch: 2.589645, Roll: 4.119998
Quaternion: [W=-0.024422, X=-0.034713, Y=-0.052819, Z=0.997702]
Gravity: [X=-0.071846, Y=0.045066, Z=-0.996397]
Linear Acceleration: [X=0.389371, Y=-0.279760, Z=8.885352]
Heading: 5.967731
Heading Error: 0.106927
==============================
mag: [-0.115000, 0.807000, 0.649000]
acc: [9.217143, 0.588634, 0.117248]
gyro: [-0.707075, -0.092699, -0.029016]
Yaw: 6.942193, Pitch: 0.362013, Roll: 3.827046
Quaternion: [W=-0.005173, X=-0.033138, Y=-0.060616, Z=0.997598]
Gravity: [X=-0.066745, Y=0.006304, Z=-0.997750]
Linear Acceleration: [X=0.521889, Y=0.123552, Z=8.219393]
Heading: 6.942193
Heading Error: 0.091870
==============================
mag: [0.053000, 0.789000, 0.685000]
acc: [9.414551, 0.581455, -0.057428]
gyro: [-1.808310, -0.272140, 0.388510]
Yaw: 7.401766, Pitch: 0.368290, Roll: 3.591856
Quaternion: [W=-0.005229, X=-0.031067, Y=-0.064616, Z=0.997413]
Gravity: [X=-0.062649, Y=0.006415, Z=-0.998015]
Linear Acceleration: [X=0.518807, Y=-0.051012, Z=8.416535]
Heading: 7.401766
Heading Error: 0.089419
==============================

 

//with 9x

mag: [0.056000, 0.906000, 0.580000]
acc: [9.843464, 0.562313, 0.478564]
gyro: [0.030390, 0.082467, 0.527176]
Yaw: 0.548519, Pitch: -2.783378, Roll: 3.265410
Quaternion: [W=0.024141, X=-0.028600, Y=-0.004091, Z=0.999291]
Gravity: [X=-0.056961, Y=-0.048481, Z=-0.997199]
Linear Acceleration: [X=0.505351, Y=0.430083, Z=8.846266]
Heading: 0.548519
Heading Error: 0.100627
==============================
mag: [0.026000, 0.921000, 0.583000]
acc: [9.811160, -0.222532, 1.222133]
gyro: [0.006414, 1.013576, 0.492967]
Yaw: 3.713483, Pitch: -7.100546, Roll: -1.289394
Quaternion: [W=0.062252, X=0.009218, Y=-0.033033, Z=0.997471]
Gravity: [X=0.022502, Y=-0.123580, Z=-0.992079]
Linear Acceleration: [X=-0.200030, Y=1.098553, Z=8.819080]
Heading: 3.713483
Heading Error: 0.049027
==============================
mag: [0.059000, 0.945000, 0.547000]
acc: [9.217143, -0.576670, 0.567098]
gyro: [-0.872772, 0.035125, 0.729219]
Yaw: 10.832839, Pitch: -3.520864, Roll: -3.573319
Quaternion: [W=0.033510, X=0.028126, Y=-0.095257, Z=0.994491]
Gravity: [X=0.062326, Y=-0.061293, Z=-0.996172]
Linear Acceleration: [X=-0.514344, Y=0.505806, Z=8.220971]
Heading: 10.832839
Heading Error: 0.064499
==============================
mag: [0.191000, 0.963000, 0.472000]
acc: [10.156923, -0.013759, 3.787236]
gyro: [-1.945602, 0.439211, -0.312762]
Yaw: 13.846349, Pitch: -20.449083, Roll: -0.072748
Quaternion: [W=0.176287, X=-0.020776, Y=-0.118736, Z=0.976930]
Gravity: [X=0.001270, Y=-0.349375, Z=-0.936982]
Linear Acceleration: [X=-0.012489, Y=3.437861, Z=9.219941]
Heading: 13.846349
Heading Error: 0.046600
==============================
mag: [0.083000, 0.939000, 0.535000]
acc: [9.631699, -0.590428, 0.399003]
gyro: [-0.426230, 0.458759, 0.186466]
Yaw: 13.611735, Pitch: -2.372174, Roll: -3.504874
Quaternion: [W=0.024167, X=0.027907, Y=-0.119053, Z=0.992201]
Gravity: [X=0.061133, Y=-0.041313, Z=-0.997274]
Linear Acceleration: [X=-0.529295, Y=0.357690, Z=8.634424]
Heading: 13.611735
Heading Error: 0.064753
==============================