Skip to main content
Associate III
January 19, 2024
Solved

Response time of LPS sensor

  • January 19, 2024
  • 1 reply
  • 914 views

Hello,

 "1/ODR (1 à 200 HZ)" is it the response time of the sensor ?

Thank you 

This topic has been closed for replies.
Best answer by Federica Bossi

Hi @ljm ,

What do you mean with "response time"? 

If I understood properly the data is ready every ODR so you can read it every 1/ODR seconds.

 

1 reply

Federica Bossi
Federica BossiBest answer
Technical Moderator
January 19, 2024

Hi @ljm ,

What do you mean with "response time"? 

If I understood properly the data is ready every ODR so you can read it every 1/ODR seconds.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
ljmAuthor
Associate III
March 14, 2024

Hi @Federica Bossi  

I'm currently using your LPS22DFmodule to measure pressure and I saw in the datasheet that the temperature accuracy is  ±1.5 °C (T = 0 to 80°C). My working range is between -15°C and 60°C. Could you please give me the accuracy of this sensor in the range -15 to 65°C?