Skip to main content
Associate II
August 12, 2024
Question

Run time fault detection in ASM330LHB

  • August 12, 2024
  • 1 reply
  • 711 views

Hi,

    I am using ASM330LHB in my project. ASM330LHB has only built self test which can only executed during power on to see ASM330LHB is healthy or faulty? But during runtime (device working in dynamic conditions) there is no way to find ASM330LHB is healthy or faulty?

1. Please suggest a method to find ASM330LHB is healthy or faulty during runtime?

2. Is ASM330LHB is fully calibrated against over its temperature range?

Thanks in advance,

Pavani.

 

 

1 reply

Federica Bossi
Technical Moderator
September 2, 2024

Hi @Pavani ,

The self test works only in static conditions.

I confirm that ASM330LHB is calibrated over the entire temperature range.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
PavaniAuthor
Associate II
September 12, 2024

Hi, Thank you for your reply. How many times we can perform self test (in static condition) for ASM330 in its lifetime? Is there any limit OR can we perform self test unlimited times? If there is any limit please mention the count.

Thanks in Advance,

Pavani