Skip to main content
Associate II
January 22, 2024
Question

Sensor Fusion Performance of LSM6DSV16X

  • January 22, 2024
  • 1 reply
  • 964 views

Hi all, 

I am trying to program my LSM6DSV16X sensor to operate with its embedded SFLP capabilities. The datasheet for the sensor describes there being three sensor fusion performance operating regions: static accuracy, low dynamic accuracy, and high dynamic accuracy. 

Is there a configuration of the LSM6DSV16X sensor that is best suited to facilitate each of the accuracy modes, specifically I am interested in the Low Dynamic Accuracy region of operation? Is there an ideal configuration to achieve this operational accuracy? Or are these more guidelines as to how the accuracy of the board will react to different speeds of motion regardless of the configuration of the board? 

ZoeTakacs_0-1705949009864.png

Any insight on this matter is appreciated! Thanks in advance!

This topic has been closed for replies.

1 reply

Federica Bossi
Technical Moderator
January 23, 2024

Hi @ZoeTakacs ,

It is difficult to answer because sensor fusion performance depends from scenario to scenario.

You can try setting a 120 Hz ODR and setting the lowest FS for the application you need.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.