Skip to main content
Associate
March 18, 2025
Solved

Sensor Tile Box Pro connection problems with pc

  • March 18, 2025
  • 1 reply
  • 860 views

Hello, community!

I recently purchased the SensorTile Box Pro to conduct various educational experiments. It connects via Bluetooth to my phone, but when I try to connect it to my laptop using the MEMS STUDIO application, it does not work via either USB or Bluetooth. I receive a red error message stating that the board is not identified.

I have tried on three different PCs, both on Windows 10 and Windows 11, but it still does not work. All the necessary drivers have been installed, and I have no explanation for why it is not being recognized. I should mention that my laptop is running Windows 10.

Can you help me?

Best answer by Federica Bossi

Hi @Ats6 ,

In order to connect the STEVAL MKBOXPro to MEMS Studio, you have to either upload the dedicated FW in the Firmware folder of MEMS Studio (USB c serial communication) or create the FW with Algobuilder to communicate via Bluetooth. It cannot use the FW compatible with the mobile app.

1 reply

Federica Bossi
Federica BossiBest answer
Technical Moderator
April 10, 2025

Hi @Ats6 ,

In order to connect the STEVAL MKBOXPro to MEMS Studio, you have to either upload the dedicated FW in the Firmware folder of MEMS Studio (USB c serial communication) or create the FW with Algobuilder to communicate via Bluetooth. It cannot use the FW compatible with the mobile app.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Ats6Author
Associate
April 10, 2025

Hi @Federica Bossi! Is there any tutorial or topic on this topic? I'm a beginner with the platforms and devices from stmicroelectronics and something more concrete and easy to understand could help me. Thank you!