Skip to main content
Joerg Wagner
Senior III
October 18, 2024
Solved

STEVAL-Proteus1 many issues in demo App

  • October 18, 2024
  • 1 reply
  • 1452 views

I tried all 3 available demos: default, FP-AI and Datalogger.

At last I flashed the original default demo back. All tests are done USB-powered or with LiPo.

Establishing a BLE connection with iPhone works in 10% of the cases.

Using an Android smartphone is more successfully.

All issues found:

- No plot data of gyro and accelerometer, but FFT and Board Pred Maintenance worked.

- In plot data the axes and 3 colored lines were shown at zero level, but no lines are changing (regardless autoscale setting).

- FFT shows sometimes lines horizontically like in plot data, no vertical bars and frozen.

- Or no sensor data at all, but I can turn on/off LED (very nice)

- Or plot data does not scroll, lines were drawn back and forth

- BLE interrupted on iPhone

 

Version FW: WB5MMG_STSW-PROTEUS_1.1.0 (from STEVAL-Proteus1 package) BLE-CbM

Having the latest BLE stack from Github (V1.20.0 build 2), because one ST employee noticed an older one (V1.19.0) in the current STEVAL-Proteus1 package. 

I tried to show the demo to a customer in their factory and it ended not well.

Do I have to wait for STEVAL-Proteus 1.2.0 ?

Best regards

 

 

Best answer by Federica Bossi

Hi @Joerg Wagner ,

The new STSW-PROTEUS v1.1.1 release is available on st.com

(STSW-PROTEUS - Software package for the STEVAL-PROTEUS1 kit with signal processing to enable predictive maintenance in a WPAN - STMicroelectronics)

I suggest you update the BLE stack to version 1.19.0 to enable the low-power functionality used by STSW-PROTEUS.

Note that after installing STSW-PROTEUS v1.1.1 via FUOTA, you need to power off the board.

1 reply

Federica Bossi
Federica BossiBest answer
Technical Moderator
November 13, 2024

Hi @Joerg Wagner ,

The new STSW-PROTEUS v1.1.1 release is available on st.com

(STSW-PROTEUS - Software package for the STEVAL-PROTEUS1 kit with signal processing to enable predictive maintenance in a WPAN - STMicroelectronics)

I suggest you update the BLE stack to version 1.19.0 to enable the low-power functionality used by STSW-PROTEUS.

Note that after installing STSW-PROTEUS v1.1.1 via FUOTA, you need to power off the board.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Joerg Wagner
Senior III
November 14, 2024

Hi Federica,

Thank you for the information.

Looks good!

All issues I mentioned are fixed with STSW-PROTEUS1 v1.1.1.

I suggest to use the BLE stack version 1.20.0 from Github project STM32CubeWB, released 5 months ago.

Version 1.19.0 would be a downgrade, not an upgrade.

Best regards