STEVAL-STWINBX1: BleSensors App = Cannot Connect via BLE
- June 30, 2023
- 2 replies
- 2262 views
I recently received the STEVAL-STWINBX1 and plugged it in out of the box and it worked fine. There was a firmware update which I did successfully.
Next, I downloaded FP-SNS-STBOX1 v1.5.0 to test it out. As per the readme I imported the "STM32CubeFunctionPack_STBOX1_V1.5.0\Projects\STWIN.box\Applications\BLESensors" into STM32CubeIDE and built the application in release mode. Following UM2965 I programmed the binary via USB DFU mode. It programs successfully but when I go to use the ST BLE Sensor app on my iPhone it can see the STWinBX device but fails with a "Cannot connect with the device: STWinBX" error message.
In the iPhone ST BLE Sensor application I noticed that it still reports the default firmware on Bank 2.....it doesn't seem to show the new BLESensors app. Screenshot and programming log attached for reference.
Any troubleshooting tips? I didn't change anything in the BLESensors app, just imported, compiled, and programmed. Don't know what I'm missing but clearly I messed something up.
Thank you very much!