Skip to main content
joe_electric
Visitor II
July 25, 2024
Question

STHS34PF80 - Can interrupt generation be non-volatile programmed?

  • July 25, 2024
  • 1 reply
  • 763 views

I would like the ability to generate an interrupt be programmed into the embedded flash so that I can use STHS34PF80 without a microcontroller. Is this possible?

1 reply

Federica Bossi
Technical Moderator
July 26, 2024

Hi @joe_electric ,

STHS34PF80 has no embedded flash. You need a microcontroller to configure it, and then you can keep the microcontroller in sleep mode while the sensor is working.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.