Skip to main content
TPhil.3
Associate
April 14, 2025
Solved

STHS34PF80TR INT pin Source / Sink capability?

  • April 14, 2025
  • 1 reply
  • 350 views

Greetings - what are the recommended maximum current ratings for the INT pin in either Push-Pull or Open-Drain? And FWIW, I was really surprised NOT to find this published in the datasheet...

TIA,

-Terry

Best answer by Federica Bossi

Hi @TPhil.3 ,

The interrupt pin can sink maximum 4mA.

Consider that the interrupt pins are usually connected directly to a microcontroller and are not made to drive load (e.g., LEDs).

1 reply

Federica Bossi
Federica BossiBest answer
Technical Moderator
April 18, 2025

Hi @TPhil.3 ,

The interrupt pin can sink maximum 4mA.

Consider that the interrupt pins are usually connected directly to a microcontroller and are not made to drive load (e.g., LEDs).

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.