Skip to main content
carton
Associate II
December 8, 2022
Solved

STPM33 : VREF1 and VREF2

  • December 8, 2022
  • 1 reply
  • 1356 views

Hi,

I'm working on a design with a STPM33. The application only needs to measure current on a single phase but, as STPM33 seems cheaper than STPM32, this was the chosen IC.

0693W00000WKWHvQAP.png  

Could I remove C27 and C28 if the second channel is not used? If yes, could I let the VREF2 floating or should I do something with it?

Thanks for your help.

This topic has been closed for replies.
Best answer by carton

I've found the answer in the datasheet:0693W00000WKWJwQAP.png

1 reply

carton
cartonAuthorBest answer
Associate II
December 8, 2022

I've found the answer in the datasheet:0693W00000WKWJwQAP.png