Skip to main content
Associate III
August 30, 2024
Question

tap detection query in lsm6dso

  • August 30, 2024
  • 1 reply
  • 532 views

I want the tap detection to work only in x axis, so I have set the TAP_Y_EN and TAP_Z_EN to 0.
But still im able to see in the logs like interrupt from z and y. 
I'm using the api lsm6dso_tap_detection_on_y_set, lsm6dso_tap_detection_on_z_set and passing 0. 

1 reply

VarshaAuthor
Associate III
September 2, 2024

Any updates on the above query? 

 

I want the tap detection to work only in x axis, so I have set the TAP_Y_EN and TAP_Z_EN to 0.
But still im able to see in the logs like interrupt from z and y. 
I'm using the api lsm6dso_tap_detection_on_y_set, lsm6dso_tap_detection_on_z_set and passing 0.