Skip to main content
Visitor II
February 6, 2024
Solved

tolerance of IMU internal clock sampling frequency

  • February 6, 2024
  • 1 reply
  • 984 views

Hi,

I am using IMU sensor LSM6DSO set to 100 Hz sampling rate. I am trying to figure out what is the tolerance of the IMU sampling frequency set by it's internal clock. How confident can I be that when I set it to 100 Hz, it will not fluctuate to higher/lower frequencies?

This topic has been closed for replies.
Best answer by Federica Bossi

Hi @zce ,

From characterization data, and thus not guaranteed in production, the ODR Error percentage is between +/- 15%.

1 reply

Federica Bossi
Federica BossiBest answer
Technical Moderator
February 7, 2024

Hi @zce ,

From characterization data, and thus not guaranteed in production, the ODR Error percentage is between +/- 15%.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.