Skip to main content
Visitor II
October 31, 2023
Question

Unable to read registers from ISM330IS

  • October 31, 2023
  • 1 reply
  • 1037 views

Hello,

 

I am trying to get a ISM330IS IMU working. I have ordered a development kit from Mouser / ST Micro with the following board number https://www.mouser.in/ProductDetail/STMicroelectronics/STEVAL-MKI230KA?qs=amGC7iS6iy%252B%252BWAEBNHSnWw%3D%3D (photos are also attached).

 

sa32953_0-1698726755935.png

 

I have done the wiring referring to the User Manual Section 5.1. (photo is also attached). I am using a I2C to USB converter (photo is attached below) to read the data in a linux based Ubuntu 22.04 PC via library i2c-dev.

Link to User Manual I am following: https://www.st.com/resource/en/datasheet/ism330is.pdf

 

sa32953_1-1698726776353.png

 

sa32953_2-1698726776150.png

 

 

I am able to connect to the I2C bus and connect to Slave Address as per User Manual Section 5.1.1.1.

 

I am facing a problem: 

  1. When I am trying to read the IMU data through any register (for Temperature sensor or WHO_AM_I from user manual page 30), all the values are coming out to be zero constantly. I am unsure what the reason for this is. (I am not getting any kind of runtime errors).

 

Does someone have an idea why this could happen? Perhaps I am missing something to start the communication via I2C. Or something needs to be triggered before I start reading these registers on the sensor hub?

 

Here’s the code I am using:

 

 

void connect_i2c(std::shared_ptr<rclcpp::Node> imu_node){

		const char* i2cDevice = "/dev/i2c-1"; // I2C bus number
		
		i2cFile = open(i2cDevice, O_RDWR);

		// Open the I2C device file for reading
		if (i2cFile < 0) {
			perror("Failed to open the I2C device.");
		}
		else{
			std::cout << "I2C open successful" << "\n";
		}

 const uint8_t i2cAddress = 0b1101010; // I2C device's address

 if (ioctl(i2cFile, I2C_SLAVE, i2cAddress) < 0) {
			perror("Failed to set I2C address.");
		}	
		else{
			std::cout << "Slave open successful" << "\n";
		}

		// Write a command or data to initiate communication 
 //(replace 0x01 with your specific command)
		unsigned char command = 0x00;
		if (write(i2cFile, &command, 1) != 1) {
			std::cerr << "Failed to write data to the ISM330IS sensor" << std::endl;	
		}

 // This will run iteratively
		run_i2c(imu_node);
}


void run_i2c(std::shared_ptr<rclcpp::Node> imu_node){
		sleep(2);
		rclcpp::Rate loop_rate(5);
		while (rclcpp::ok())
		{
 int registerToRead = 0x0F; // Replace with the register address you want to read


			if (write(i2cFile, &registerToRead, 1) != 1) {
				perror("Error writing register address");
				//return 1;
			}

			uint8_t data;
			if (read(i2cFile, &data, 1) != 1) {
				perror("Error reading data");
				//std::cerr << "Error reading data" << std::endl;
				//return 1;
			}

			std::cout << "Data from register 0x" << std::hex << registerToRead << ": 0x" << static_cast<int>(data) << std::endl;

			
 loop_rate.sleep();
			rclcpp::spin_some(imu_node);
		}

 

 

 

 

This topic has been closed for replies.

1 reply

Federica Bossi
Technical Moderator
November 3, 2023

Hi @sa32953 ,

Welcome to ST Community!

From your photos it seems that you are connecting GND of the STEVAL to SCL of your board. Can you check this?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.