Skip to main content
Visitor II
October 16, 2024
Question

Use the SPI of Nucleo-F446RE to connect to LSM9DS1

  • October 16, 2024
  • 2 replies
  • 1036 views

+I'm a beginner. I used the STM32 CubeIDE to compile and used the SPI of the Nucleo-F446RE to connect to the LSM9DS1. I want to read the data of its accelerometer, gyroscope and magnetometer, and use the field expression function to observe it. I found that the value read by it will keep beating without moving the LSM9DS1 and my magnetometer will not respond. I don't know what I did wrong.

The following is what I wrote myself about the function library and main program used by LSM9DS1.

[SPI_IMU_LSM9DS1.h]

 

#include "stm32f446xx.h"

#include "stm32f4xx_hal.h"

#include "stdint.h"

#include "stdio.h"

#include "stdlib.h"



#ifndef INC_SPI_IMU_LSM9DS1_H_

#define INC_SPI_IMU_LSM9DS1_H_



#define CS_AG_PORT GPIOA

#define CS_AG_PIN GPIO_PIN_0

#define CS_M_PORT GPIOA

#define CS_M_PIN GPIO_PIN_1

#define DEN_AG_PIN GPIO_PIN_2



// Magnetometer Register address (CS_M low level)

#define WHO_AM_I_M 0x0F // Response: 0011 1101 (0x3D)

#define OFFSET_X_REG_L_M 0x05

#define OFFSET_X_REG_H_M 0x06

#define OFFSET_Y_REG_L_M 0x07

#define OFFSET_Y_REG_H_M 0x08

#define OFFSET_Z_REG_L_M 0x09

#define OFFSET_Z_REG_H_M 0x0A

#define CTRL_REG1_M 0x20

#define CTRL_REG2_M 0x21

#define CTRL_REG3_M 0x22

#define CTRL_REG4_M 0x23

#define CTRL_REG5_M 0x24

#define OUT_X_L_M 0x28

#define OUT_X_H_M 0x29

#define OUT_Y_L_M 0x2A

#define OUT_Y_H_M 0x2B

#define OUT_Z_L_M 0x2C

#define OUT_Z_H_M 0x2D



// Define function type

int8_t IMU_spiRead_9D(SPI_HandleTypeDef *hspi, uint8_t address, uint8_t measurer);

void IMU_spiWrite_9D(SPI_HandleTypeDef *hspi, uint8_t address, uint8_t data, uint8_t measurer);

int8_t IMU_configure_9D(SPI_HandleTypeDef *hspi);

int16_t Check_ID(SPI_HandleTypeDef *hspi);

#endif /* INC_SPI_IMU_LSM9DS1_H_ */

 

 

[SPI_IMU_LSM9DS1.c]

 

#include "stdio.h"

#include "stdlib.h"

#include "SPI_IMU_LSM9DS1.h"

#include "main.h"



int8_t IMU_configure_9D(SPI_HandleTypeDef *hspi)

{

// IMU_spiWrite_9D(SPI_HandleTypeDef *hspi, uint8_t address, uint8_t data, uint8_t measurer);

//PC0 = 0;

//int8_t data1;

//IMU_spiWrite_9D(CTRL_REG8,0x01,1); //1100 0001

//interrupt

IMU_spiWrite_9D(hspi, 0x06, 0x3F, 1); // 0011 1111

IMU_spiWrite_9D(hspi, 0x30, 0x3F, 1); // 0011 1111

// IMU configure gyroscope accelerometer

IMU_spiWrite_9D(hspi, CTRL_REG1_G, 0x78, 1); //0101 1100 2000dps ODR=199Hz cut-off=14Hz (after LPF1)(after LPF2) //011 1 1000

// when both Gyro and Accel enabled, Both ODR only be set here!

// 110 11 0 11 = 1101 1011

IMU_spiWrite_9D(hspi, CTRL_REG2_G, 0x00, 1); //0000 0000 //0000 0000

//LP_mode HP_EN 0(1)1 0(1) HPCF3_G HPCF2_G HPCF1_G HPCF0_G

IMU_spiWrite_9D(hspi, CTRL_REG3_G, 0x48, 1); //0000 0000 HP filter // 0000 1000

IMU_spiWrite_9D(hspi, ORIENT_CFG_G, 0x00, 1); //0000 0000

IMU_spiWrite_9D(hspi, 0x14, 0x00, 1);

IMU_spiWrite_9D(hspi, CTRL_REG4, 0x38, 1); //0011 1000 output enabled, interrupt

IMU_spiWrite_9D(hspi, CTRL_REG5_XL, 0x78, 1); // 01 1 1 1 000 decimation?

IMU_spiWrite_9D(hspi, CTRL_REG6_XL, 0x16, 1); // 000 10 1 10 "0x10"ODR_XL=0Hz(ODR=119Hz) BW=408Hz BW selected by ODR +-4g //011 11 0 00

//ODR_XL only enable when "only-Accel mode":1101 0000 ODR_XL=952Hz BW=408Hz BW selected by ODR

IMU_spiWrite_9D(hspi, CTRL_REG7_XL, 0x02, 1); //0000 0010 HR=1 DCF=10 LP cutff=ODR/9

IMU_spiWrite_9D(hspi, CTRL_REG8, 0x40, 1); // 0100 0000 last bit is reset 0000 0100

IMU_spiWrite_9D(hspi, CTRL_REG9, 0x07, 1); // 0000 0111

IMU_spiWrite_9D(hspi, 0x2E, 0x00, 1); //000 0 0001

// end



// IMU configure Magnetometer

IMU_spiWrite_9D(hspi, CTRL_REG1_M, 0x62, 0); //0 11 000 1 0 temperature com not using,ultra mode,Fast_ODR disabled 0010 0010

IMU_spiWrite_9D(hspi, CTRL_REG2_M, 0x60, 0); //0 11 0 0 0 0 00 +-16 gauss bit2 is reset operation //+-4 cause error ,10 +-12, 01 +-8, 00 +-4

IMU_spiWrite_9D(hspi, CTRL_REG3_M, 0x80, 0); //1 0 0 00 0 00 I2C_DISABLE,SPI read&write,Operating mode=Single-conversion mode %%%%%%%%% SIM opposite 1000 0000

IMU_spiWrite_9D(hspi, CTRL_REG4_M, 0x0C, 0); //0000 11 00

IMU_spiWrite_9D(hspi, CTRL_REG5_M, 0x00, 0); //0100 0000



return 0;

}





int16_t Check_ID(SPI_HandleTypeDef *hspi)

{

return IMU_spiRead_9D(hspi, WHO_AM_I_AG, 1); // Read the ID of the accelerometer/gyroscope

}





void IMU_spiWrite_9D(SPI_HandleTypeDef *hspi, uint8_t address, uint8_t data, uint8_t measurer)

{

uint8_t txData[2] = {address & ~0x80, data}; // Write operation, clear RW bit



if (measurer == 1) // Accelerometer/Gyroscope

{

HAL_GPIO_WritePin(CS_AG_PORT, CS_AG_PIN, GPIO_PIN_RESET); // Pull CS_AG low

HAL_SPI_Transmit(hspi, txData, 2, HAL_MAX_DELAY); // Send data

while (HAL_SPI_GetState(hspi) != HAL_SPI_STATE_READY); // wait

HAL_GPIO_WritePin(CS_AG_PORT, CS_AG_PIN, GPIO_PIN_SET); // Pull up CS_AG

}

else // Magnetometer

{

HAL_GPIO_WritePin(CS_M_PORT, CS_M_PIN, GPIO_PIN_RESET); // Pull CS_M low

HAL_SPI_Transmit(hspi, txData, 2, HAL_MAX_DELAY); // Send Data

while (HAL_SPI_GetState(hspi) != HAL_SPI_STATE_READY); // wiat

HAL_GPIO_WritePin(CS_M_PORT, CS_M_PIN, GPIO_PIN_SET); // Pull up CS_M

}

}



int8_t IMU_spiRead_9D(SPI_HandleTypeDef *hspi, uint8_t address, uint8_t measurer)

{

uint8_t txData = address | 0x80; // Read operation, set RW bit

uint8_t rxData = 0;



if (measurer == 1) // Accelerometer/Gyroscope

{

HAL_GPIO_WritePin(CS_AG_PORT, CS_AG_PIN, GPIO_PIN_RESET); // 拉低CS_AG

HAL_SPI_Transmit(hspi, &txData, 1, HAL_MAX_DELAY); // 發送地址

while (HAL_SPI_GetState(hspi) != HAL_SPI_STATE_READY);

HAL_SPI_Receive(hspi, &rxData, 1, HAL_MAX_DELAY); // 接收數據

while (HAL_SPI_GetState(hspi) != HAL_SPI_STATE_READY);

HAL_GPIO_WritePin(CS_AG_PORT, CS_AG_PIN, GPIO_PIN_SET); // 拉高CS_AG

}

else // Magnetometer

{

HAL_GPIO_WritePin(CS_M_PORT, CS_M_PIN, GPIO_PIN_RESET); // 拉低CS_M

HAL_SPI_Transmit(hspi, &txData, 1, HAL_MAX_DELAY); // 發送地址

while (HAL_SPI_GetState(hspi) != HAL_SPI_STATE_READY);

HAL_SPI_Receive(hspi, &rxData, 1, HAL_MAX_DELAY); // 接收數據

while (HAL_SPI_GetState(hspi) != HAL_SPI_STATE_READY);

HAL_GPIO_WritePin(CS_M_PORT, CS_M_PIN, GPIO_PIN_SET); // 拉高CS_M

}



return rxData;

}

 

 

 

 

 

 

2 replies

mƎALLEm
Technical Moderator
October 16, 2024

Hello @Jian003 and welcome to the community,

Please use </> button to paste your code. You can refer to our tips on posting on this link. I'm editing your post then.

Thank you for your understanding.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
Federica Bossi
Technical Moderator
October 23, 2024

Hi @Jian003 ,

You can look at our official drivers on Github.

Let me know if this helps.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.