Skip to main content
Andrea Verdecchia
Associate II
October 9, 2024
Solved

What is the best magnetometer to pair with the LSM6DSV16X

  • October 9, 2024
  • 1 reply
  • 1325 views

I have to work on a project that includes an accelerometer, gyroscope, and magnetometer. For the first two, I would like to use the LSM6DSV16X sensor, but I haven't yet chosen a magnetometer.

1) Do you have any recommendations for one that would work well with the LSM6DSV16X?

2) Is it possible to synchronize the sampling between the LSM6DSV16X and the magnetometer?

Best answer by Federica Bossi

Hi @Andrea Verdecchia ,

You could look at LIS2MDL.

If you want to compute sensor hub with LSM6DSV16X you can follow this official example on Github and the section 7 of AN5763.

Hope this helps :)

1 reply

Federica Bossi
Federica BossiBest answer
Technical Moderator
October 9, 2024

Hi @Andrea Verdecchia ,

You could look at LIS2MDL.

If you want to compute sensor hub with LSM6DSV16X you can follow this official example on Github and the section 7 of AN5763.

Hope this helps :)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Andrea Verdecchia
Associate II
October 21, 2024

Thank you for your suggestion. Do you know if I can find an example schematic somewhere showing the interconnection between the LSM6DSV16X and the LIS2MDL, like the schematic of a development board that has both of them?

Thanks anyway. 

Federica Bossi
Technical Moderator
October 23, 2024

Hi @Andrea Verdecchia ,

We don't have LSM6DSV16X and LIS2MDL, but we have MKI217V1 that has LSM6DSO which is pin-pin compatible with LSM6DSV16X. So I think you could look at this schematic

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.