Skip to main content
SBroc.1
Visitor II
May 10, 2023
Question

What size of O-Ring and bore hole would you recommend for mounting the ILPS28QSW sensor wather tight?

  • May 10, 2023
  • 1 reply
  • 1097 views

..

    This topic has been closed for replies.

    1 reply

    Associate II
    July 6, 2023

    See documentation for the lps28dfw, application note: AN5937

    Associate III
    January 23, 2024

    AN5937 indeed has the dimensions for the o-ring (see Fig. 3).  1.8mm inner diameter, 0.5mm cross-section diameter.

    But here's a snag: the smallest standard cross-section diameter is 1mm (from these tables). 

    Who makes the appropriate non-standard o-rings?  Please post the suppliers and the part numbers.