Skip to main content
This topic has been closed for replies.
Best answer by Luca SEGHIZZI

LSM6DSV16X has an enhanced AI in-the edge with machine-learning core (MLC), Final state machine (FSM)), while for local processing has a sensor fusion low-power algorithm, an on-the-fly self-configuration, pedometer and an electrostatic sensing (Qvar). These advanced MEMS sensors drive the intuitive context-aware features of today’s battery-operated applications.

1 reply

Luca SEGHIZZI
Luca SEGHIZZIBest answer
Senior
February 17, 2023

LSM6DSV16X has an enhanced AI in-the edge with machine-learning core (MLC), Final state machine (FSM)), while for local processing has a sensor fusion low-power algorithm, an on-the-fly self-configuration, pedometer and an electrostatic sensing (Qvar). These advanced MEMS sensors drive the intuitive context-aware features of today’s battery-operated applications.