Skip to main content
WGebh.1
Visitor II
February 14, 2023
Question

Which hardware solution can be recommended for recording from digital MEMS microphones?

  • February 14, 2023
  • 1 reply
  • 1037 views

I would like to use the digital interface (not sure what that means) of an existing system control computer to control the recording (start & stop, perhaps gain etc.) from digital MEMS microphones (I2S or PDM). Which hardware options do I have, and how could I control the recording via scripting etc.?

This topic has been closed for replies.

1 reply

Eleon BORLINI
ST Employee
February 14, 2023

Hi @WGebh.1​ ,

For a direct acquisition with PC (through UART / USB) of a digital MEMS microphone (PDM), my suggestion is to use the X-NUCLEO ecosystem, and in particular the X-NUCLEO-CCA02M2 board. You can plug for example the STEVAL-MIC006V1 in the 6-pin headers. This is general purpose hardware. If you need a more specific application, you might have a look at this list.

-Eleon