Skip to main content
lectric
Associate
May 16, 2023
Solved

X-CUBE-TOF1 v3.3 VL53L4CX library compilation issue when the raw project is built.

  • May 16, 2023
  • 1 reply
  • 1121 views

The library of VL53L4CX returns me a fatal error with the message no such file or directory, but the file it refers is in another directory of the same project. The project is just created and the error appears, can it be a bug or some problem with the library? Thank you

In file included from ../Drivers/BSP/Components/vl53l4cx/porting/vl53lx_platform_ipp.c:15:
../Drivers/BSP/Components/vl53l4cx/porting/vl53lx_platform_ipp.h:17:10: fatal error: vl53lx_platform_user_data.h: No such file or directory
 17 | #include <vl53lx_platform_user_data.h>
 | ^~~~~~~~~~~~~~~~~~~~~~~~~~~~~
compilation terminated.

This topic has been closed for replies.
Best answer by lectric

I solved the problem reading another question. The solution is to add paths to the project following this method:

right click project -> Properties -> C/C++ Build -> Settings -> Tool Settings -> MCU GCC Compiler -> Include paths

1 reply

lectric
lectricAuthorBest answer
Associate
May 16, 2023

I solved the problem reading another question. The solution is to add paths to the project following this method:

right click project -> Properties -> C/C++ Build -> Settings -> Tool Settings -> MCU GCC Compiler -> Include paths