Skip to main content
KiptonM
Senior III
July 15, 2022
Solved

Blue Pill: Application crashing debugger; unable to reset in the debugger.

  • July 15, 2022
  • 8 replies
  • 6611 views

What would cause an application to crash the debugger and not be able to reset in the debugger, without exiting the debugger?

 

I am just about finished with my application I have been working on for a few months.

The processor is a STM32G051K8T and I have upgraded to STMCubeIDE 1.10.1 and am using the ST-LINK V2 (Blue pill) with my custom board.

 

All of a sudden it is hanging up in the main program.

At first it hung up in the middle of a sprintf() statement.

The statement was

 char buf[120];
	 sprintf(buf,"Calibration Factor: %lu\r\n",ADC1->CALFACT); // dies on this statement
	 print_debug_str("Hello World\r\n");

 

char buf[120] was originally char buf[40] but I made it longer in the unlikely case it was overrunning the buffer. Made no difference.

 

I changed "ADC1-CALFACT" to "16l" or "(uint32_t) 16" made no difference. it just hung on that command.

 

Since I new sprintf probably used the heap, I went into STM32G051K8TX.ld to maje the minimum heap 0x300 from 0x200. And it made no difference.

 

My first thought was it is happening at a certain memory location. So I put 100 __NOP(); statements before the code that had the sprintf() in it. Did not matter, it still hung up on the sprintf()

 

I commented out the sprintf() statement and changed the  print_debug_str(buf); to

 print_debug_str("Hello World\r\n"); and it hung up in the print_debug str() routine.

 

void print_debug_str(void * s)
{
	static uint8_t db[256];
	volatile uint32_t i = 0;
	volatile uint32_t j;
	uint16_t len = strlen(s);
	while (UART1Busy) i++;
	memmove(db,s,len);
	UART1Busy = true;
	for (j=0;j<2500;j++) i++; // now stopping here
	HAL_UART_Transmit_DMA(&huart1,db,len);
}
 
void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart)
{
	UART1Busy = false;
	UNUSED(huart);
}

That made me wonder if it was not memory based but time based.

 

So I put the 100 __NOP(); in a for loop;

{
	 uint16_t i;
	 for (i=0;i<30000;i++)
	 {
		 __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); // 20
		 __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); // 40
		 __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); // 60
		 __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); // 80
		 __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); // 100
	 }
 }

Now it stops in this code before the sprintf() statement.

 

I am now guessing it is a time issue. It happens at a certain time.

I have never setup the watchdog timer and I do use three timers (TIM2, TIM3, TIM14) later in the program. So just incase they are now not working like they used to, I decided to comment them out, which caused a warning about the routines not being called.

 

Here is the current version of the code. Until it breaks:

 

int main(void)
{
 /* USER CODE BEGIN 1 */
 
 /* USER CODE END 1 */
 
 /* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_ADC1_Init();
 MX_I2C1_Init();
 //MX_TIM2_Init();
 //MX_TIM3_Init();
 //MX_TIM14_Init();
 MX_USART1_UART_Init();
 MX_USART2_UART_Init();
 
 /* Initialize interrupts */
 MX_NVIC_Init();
 /* USER CODE BEGIN 2 */
 
 /*
 ENCODER_POWER_OFF; // Make sure encoder is off so it can start correctly.
 print_debug_str("Encoder Power Off\r\n");
 
 
 
 TASK_PIN_L;
 TP2_L;
 DIO2_L;
 DIO3_L;
 DIO4_L;
 
 if (isDebug(DEBUG_verify_memory_structures))
 {
	 verify_memory_structures();
 }
*/
 __NOP();
 {
 
	 uint16_t i;
	 for (i=0;i<30000;i++)
	 {
		 __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); // 20
		 __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); // 40
		 __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); // 60
		 __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); // 80
		 __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); // 100
	 }
 }
 //ADC_init();
 __NOP();
 
 if (HAL_ADCEx_Calibration_Start(&hadc1) != HAL_OK)
 {
	 print_debug_str("Did not calibrate right!\r\n\r\n");
 }
 else
 {
	 char buf[120];
	 sprintf(buf,"Calibration Factor: %lu\r\n",ADC1->CALFACT); // dies on this statement
	 //sprintf(buf,"Calibration Factor: %lu\r\n",(uint32_t) 0xA5A5A5A5); // dies on this statement
	 print_debug_str(buf);
 }

Maybe I need to explain what happens.

 

I run the debugger to the __NOP(); on line 55 where I have a break point, I also have a break point at the __NOP(); on line 69. When I tell it to Resume after the first breakpoint, it never returns and breaks at line 69.

 

Suspend does not appear to really work. It goes off and resume turns on, but I cannot examine variables. When I try to look at i it says "Error: Multiple errors reported.\ Failed to execute MI command: -var-create - * i Error message from debugger back end: -var-create: unable to create variable object\ Unable to create variable object"

 

trying the reset button the resume button goes out, and the suspend button lights up, but it does not go back to the beginning of main() like normal,

 

As a result, I have to use the Terminate button to leave the debugger, then Run -> Debug to get back into the debugger.

 

I upgraded to STM32CubeIDE 1.10.1 recently. Is this one of those known problems for ST in this version?

 

Did version 1.10.1 turn on something like the watchdog timer by default?

 

Any suggestions how to get past this? This has been working everyday for the past 2-3 months.

 

I have attached the whole main.c code so you can see how the peripherals were setup before this code was executed.

 

I am at a loss as to what happened. This was working. Could have something happened to the processor? I do not want to swap processors if I do not need to.

 

Thanks,

Kip

 

This topic has been closed for replies.
Best answer by KiptonM

With help from KnarfB and Piranha we finally figured out the issue in another question.

Feed Detail (st.com)

To make a long story short KnarfB noticed in one of my debugging logs that PC was wrong.

Download verified successfully 

 ------ Switching context ----- 

COM frequency = 4000 kHz

Target connection mode: Under reset

Reading ROM table for AP 0 @0xf0000fd0

Hardware watchpoint supported by the target 

ST-LINK Firmware version : V2J40S7

Device ID: 0x456

PC: 0x1fff1654

And that was in system memory not flash.

So somehow the fuses got changed. I had to load the STM32CubeProgrammer and it lets you change the fuses. Unfortunately that did not work.

Piranha noticed the fuse descriptions in the Programmer were wrong and sent me to the right place in RM0444 Paragraph 2.5, Table 8. I set the fuses based on that info and it started working. And the PC was in the right memory space.

Download verified successfully 

 ------ Switching context ----- 

COM frequency = 4000 kHz

Target connection mode: Under reset

Reading ROM table for AP 0 @0xf0000fd0

Hardware watchpoint supported by the target 

ST-LINK Firmware version : V2J40S7

Device ID: 0x456

PC: 0x8006398

Thanks all for the help.

8 replies

KiptonM
KiptonMAuthor
Senior III
July 15, 2022

That is curious. I commented out everything I was not using.

int main(void)
{
 /* USER CODE BEGIN 1 */
 
 /* USER CODE END 1 */
 
 /* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 //MX_DMA_Init();
 //MX_ADC1_Init();
 //MX_I2C1_Init();
 //MX_TIM2_Init();
 //MX_TIM3_Init();
 //MX_TIM14_Init();
 MX_USART1_UART_Init();
 //MX_USART2_UART_Init();
 
 /* Initialize interrupts */
 //MX_NVIC_Init();
 /* USER CODE BEGIN 2 */

it still crashes in the __NOP() loop.

Tesla DeLorean
Guru
July 15, 2022

sprintf() or snprintf() really don't need to use the heap, you pass them a buffer.

The ST-LINK are not, in my opinion, robust on USB Hubs, or similar arrangement on docking stations. So USB comms issues are a problem. Use of quality cables is also strongly advised.

There are no efficiency prizes for using uint16_t, the 32-bit int will be optimal for loop counts.

Do you have a Hard Fault Handler that reports failure details? The CM0(+) has a no tolerance of unaligned accesses.

Would definitely monitor stack depth. Heap probably not going to be used much of anywhere, things should fail elegantly if malloc() returns NULL. Watch for the heap/stack colliding. Large local/auto variable frequently a headache. See if problems come/go with "static" directive on larger locals. See if altering optimization levels alters behaviour, often a predictor on latent coding issues/expectations.

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
KiptonM
KiptonMAuthor
Senior III
July 18, 2022

Somehow I missed your input.

I thought the sprintf type of routines needed the heap for space to do the formatting. That is good if they do not. I think heap is a bad idea for an embedded system.

The ST-LINK-V2 is plugged directly into my laptop. No hub or cable in between.

I am just used to uint16_t for loops because I have spent so many years on 16-bit processors. And the sprintf lets you use %u as opposed to %lu. to show the variables.

I do not know what a Hard Fault Handler is or where to put it. Can you send me a link for more info?

I am using just under 30% of my RAM. So I should have plenty of stack if ST starts the stack at the top of memory and puts variables at the bottom. I increased the minimum stack by 0x100. I am not using the heap, but they have a default heap length.

Al that is good except this happens at the very beginning of the program before I call any of my routines. Right now I am just doing HAL_Init() and looping on 100 __NOP(); statements about 152 times and it crashes. No other calls. No use of the stack except for the uint16_t i; used in the loop variable. No heap. No other initializations.

And it crashes at what I believe is a call to SysTick_Handler() interrupt. It makes the debugger unusable except to terminate. And restart. I cannot pause and look at variables or anything once it crashes.

I tried single stepping and it just stops single stepping with no message in the debugger.

If I comment out the SysTic_Init the problem goes away. If I disable interrupts the problem goes away. That makes me think it is the SysTick_Handler() interrupt. But it never enters it, or the debugger does not stop at the breakpoint.

KiptonM
KiptonMAuthor
Senior III
July 15, 2022

Some new information. I double clicked on the .ioc file to bring up the MX plug-in and I have an icon spinning, and it does not bring up the MX program.

Finally it came up with a window:

0693W00000QLLwmQAH.pngThis is interesting. I did the migration, then went into the MX program to make sure everything looked O,K. It did and then I Generated the Code and recompiled, with a lot of hope.

Still stops in the __NOP(); loop.

S.Ma
Principal
July 16, 2022

Put a 500msec delay before init the peripherals.

Try your code with interrupt disable

Create interrupt routine for all unused interruptd and stick there with while 1, and put a breakpoint in there.

Check if a low power mode cut swd activity

Check if code reco figure SWD pins for non debug use

Check the stack size, increase it.

I dont use lib print, I make my own. I avoid float which is memory costly especially on cortex M0+, fixed point or Q31 format is old practicr. NO FLOAT/DOUBLE allowed within interrupts (linux and droid phone drivers know this fact). Sometime i just use int Temp_degC_x1000 to workaround float.

KiptonM
KiptonMAuthor
Senior III
July 18, 2022

I am working on your suggestions. Thanks for giving me something to try.

Put a 500msec delay before init the peripherals.

I have not needed this before, but I will try.

I put a loop in before the HAL_Init();

{

uint16_t i, j;

for (i=0;i<525;i++)

{

for (j=0;j<60000;j++) __NOP();

}

}

This is closer to 11 seconds. But it did not affect it.

Try your code with interrupt disable

I removed the delay before the initializations.

I placed __disable_irq(); after the MX_ initializations in the code, before the __NOP(); loops.

It did not hang in the __NOP(); loop. So we know now it is interrupt related.

I already tried not initializing the timers. So it must ne something else.

I commented out most of the initializations: Like so

/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 // MX_DMA_Init();
 MX_ADC1_Init();
 MX_I2C1_Init();
// MX_TIM2_Init();
// MX_TIM3_Init();
// MX_TIM14_Init();
// MX_USART1_UART_Init();
// MX_USART2_UART_Init();
 
 /* Initialize interrupts */
 MX_NVIC_Init();
 /* USER CODE BEGIN 2 */

It still is happening. I have not started I2C or ADC1 yet so I did not think they could be the issue.

So I commented them out also.

Still happening.

I commented out the MX_NVIC_Init();

Still happens.

Only thing left is MX_GPIO_Init();

Commented it out, still happens,

So now the only thing active is HAL_Init() and SystemClock_Config();

/* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
// MX_GPIO_Init();
 // MX_DMA_Init();
// MX_ADC1_Init();
// MX_I2C1_Init();
// MX_TIM2_Init();
// MX_TIM3_Init();
// MX_TIM14_Init();
// MX_USART1_UART_Init();
// MX_USART2_UART_Init();
 
 /* Initialize interrupts */
// MX_NVIC_Init();
 /* USER CODE BEGIN 2 */

I commented out SystemClock_Config(); It still happens.

I commented out HAL_Init() It does not stop in the loop. It looks like some interrupt is firing some time after HAL_Init(); is run.

But which one?

KiptonM
KiptonMAuthor
Senior III
July 18, 2022

So I am single stepping through HAL_Init();

We know the problem happens when interrupts are enabled and HAL_Init() runs.

If HAL_Init() runs and interrupts are disabled we do not have the issue.

I looks like the following things happen in HAL_Init().

__HAL_FLASH_PREFETCH_BUFFER_ENABLE();

HAL_InitTick(TICK_INT_PRIORITY)

HAL_MspInit()

As I was writing this and the system was paused at the return status for HAL_Init() the debugger stopped working. The reset button would not work.

For some reason I am thinking it is HAL_InitTick().

Because that will generate an interrupt after about 1 ms.

I started stepping through HAL_InitTick(

__weak HAL_StatusTypeDef HAL_InitTick(uint32_t TickPriority)
{
 HAL_StatusTypeDef status = HAL_OK;
 
 /* Check uwTickFreq for MisraC 2012 (even if uwTickFreq is a enum type that doesn't take the value zero)*/ 
 if ((uint32_t)uwTickFreq != 0U)
 {
 /*Configure the SysTick to have interrupt in 1ms time basis*/
 if (HAL_SYSTICK_Config(SystemCoreClock / (1000U /(uint32_t)uwTickFreq)) == 0U)
 {
 /* Configure the SysTick IRQ priority */
 if (TickPriority < (1UL << __NVIC_PRIO_BITS))
 {
 HAL_NVIC_SetPriority(SysTick_IRQn, TickPriority, 0U);
 uwTickPrio = TickPriority;
 }
 else
 {
 status = HAL_ERROR;
 }
 }
 else
 {
 status = HAL_ERROR;
 }
 }
 else
 {
 status = HAL_ERROR;
 }
 
 /* Return function status */
 return status;
}

And the debugger stopped working at the uwTickPrio = TickPriority; line.

MM..1
Chief III
July 16, 2022

Show here your it file. and other init used in MX user parts.

From quick read your UART debug is little chaos DMA .

And you test with or without ?

 ENCODER_POWER_OFF; // Make sure encoder is off so it can start correctly.
 print_debug_str("Encoder Power Off\r\n");

Plus i mean UNUSED need be first line in callback.

KiptonM
KiptonMAuthor
Senior III
July 18, 2022

I do not understand your comments.

Show here your it file.

What is "it" file?

and other init used in MX user parts.

I attached the main.c which has the MX generated initialization routines. What else do you want? I do not understand.

From quick read your UART debug is little chaos DMA .

I do not know what that means. the print_debug_str() function has been working without problem for over a year. I can print at 3047619 bps with it without an issue. I like the fast baud rate because it does not slow other things down waiting for the print.

And you test with or without ?

I am finding the problem before it is called. It appears to be time related. At first I thought it was memory position related, until I looped on the __NOP(); and it quit in there.

UNUSED() must be first line.

I have to look at the UNUSED() routine. I thought all it did was fool the compiler to think a value was used when it was not. So it did not matter where in the routine it was placed as long as the warning was not generated. I guess once the variable is used, the compiler can reuse the register in the later code when it optimizes, but in a routine so small, I doubt if you will gain more than a couple of cycles.

MM..1
Chief III
July 18, 2022

stm32??xx_it.c is for me it file.

In your mx you call

 /* USER CODE BEGIN I2C1_Init 2 */
 initI2C();
 /* USER CODE END I2C1_Init 2 */

but source dont show etc. All code started before your hang can produce it.

For example you rencoder power off is called before nop test in main and start DMA.

In parallel main continues to your test and maybe hangs because DMA etc.

KiptonM
KiptonMAuthor
Senior III
July 18, 2022

Around iteration 155 it stops responding. I am pretty sure it is the SysTick interrupt. I have a breakpoint in the interrupt and it does not break in the interrupt.

If I comment out the initialization of the SysTic in the HAL_Init the problem does not happen.

HAL_StatusTypeDef HAL_Init(void)
{
 HAL_StatusTypeDef status = HAL_OK;
 
 /* Configure Flash prefetch, Instruction cache */
 /* Default configuration at reset is: */
 /* - Prefetch disabled */
 /* - Instruction cache enabled */
 
#if (INSTRUCTION_CACHE_ENABLE == 0U)
 __HAL_FLASH_INSTRUCTION_CACHE_DISABLE();
#endif /* INSTRUCTION_CACHE_ENABLE */
 
#if (PREFETCH_ENABLE != 0U)
 __HAL_FLASH_PREFETCH_BUFFER_ENABLE();
#endif /* PREFETCH_ENABLE */
 
 /* Use SysTick as time base source and configure 1ms tick (default clock after Reset is HSI) */
 if (HAL_InitTick(TICK_INT_PRIORITY) != HAL_OK)
 {
 status = HAL_ERROR;
 }
 else
 {
 /* Init the low level hardware */
 HAL_MspInit();
 }
 
 /* Return function status */
 return status;
}

When I comment out lines 19-23 I do not have a the debugger crash.

KiptonM
KiptonMAuthor
Senior III
July 18, 2022

Here is what my code looks like at the moment:

/* USER CODE END 0 */
 
/**j
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */
/*
	{
		uint16_t i, j;
		for (i=0;i<525;i++)
		{
			for (j=0;j<60000;j++) __NOP();
		}
 
	}
*/
 /* USER CODE END 1 */
 
 /* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 //SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
// MX_GPIO_Init();
 // MX_DMA_Init();
// MX_ADC1_Init();
// MX_I2C1_Init();
// MX_TIM2_Init();
// MX_TIM3_Init();
// MX_TIM14_Init();
// MX_USART1_UART_Init();
// MX_USART2_UART_Init();
 
 /* Initialize interrupts */
// MX_NVIC_Init();
 /* USER CODE BEGIN 2 */
 
 //__disable_irq();
 /*
 ENCODER_POWER_OFF; // Make sure encoder is off so it can start correctly.
 print_debug_str("Encoder Power Off\r\n");
 
 
 
 TASK_PIN_L;
 TP2_L;
 DIO2_L;
 DIO3_L;
 DIO4_L;
 
 if (isDebug(DEBUG_verify_memory_structures))
 {
	 verify_memory_structures();
 }
*/
 __NOP();
 {
 
	 uint16_t i;
	 for (i=0;i<157;i++)
	 {
		 __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); // 20
		 __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); // 40
		 __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); // 60
		 __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); // 80
		 __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); // 100
		 if (i == 151)
		 {
			 __NOP();
		 }
	 }
 }
 //ADC_init();
 __NOP();

KiptonM
KiptonMAuthorBest answer
Senior III
July 20, 2022

With help from KnarfB and Piranha we finally figured out the issue in another question.

Feed Detail (st.com)

To make a long story short KnarfB noticed in one of my debugging logs that PC was wrong.

Download verified successfully 

 ------ Switching context ----- 

COM frequency = 4000 kHz

Target connection mode: Under reset

Reading ROM table for AP 0 @0xf0000fd0

Hardware watchpoint supported by the target 

ST-LINK Firmware version : V2J40S7

Device ID: 0x456

PC: 0x1fff1654

And that was in system memory not flash.

So somehow the fuses got changed. I had to load the STM32CubeProgrammer and it lets you change the fuses. Unfortunately that did not work.

Piranha noticed the fuse descriptions in the Programmer were wrong and sent me to the right place in RM0444 Paragraph 2.5, Table 8. I set the fuses based on that info and it started working. And the PC was in the right memory space.

Download verified successfully 

 ------ Switching context ----- 

COM frequency = 4000 kHz

Target connection mode: Under reset

Reading ROM table for AP 0 @0xf0000fd0

Hardware watchpoint supported by the target 

ST-LINK Firmware version : V2J40S7

Device ID: 0x456

PC: 0x8006398

Thanks all for the help.