Blue Pill STM32F103C8T6 not detected via ST-Link – connection/programming issue
Hello everyone,
I’m working with an STM32F103C8T6 (Blue Pill) development board and facing an issue while trying to program/debug the MCU using ST-Link V2.
Board used:
https://robocraze.com/products/stm32f103c8t6-arm-development-board
Issue details:
STM32CubeProgrammer / STM32CubeIDE does not consistently detect the target
Sometimes shows “No target connected” or fails during connection
Tried SWD mode with NRST connected
BOOT0 is set to 0 (Flash mode)
Power supplied via USB (5V) and also tested with external 3.3V
Checked SWDIO, SWCLK, GND continuity
I’m not sure if this is related to board configuration, clock settings, or ST-Link connection parameters. I’d appreciate guidance on:
Recommended ST-Link connection settings for STM32F103C8T6
Any known issues with Blue Pill boards (pull-ups, reset circuit, USB power, etc.)
Whether enabling connect under reset is mandatory for this MCU
I’m still getting familiar with the forum and STM32 ecosystem, so apologies if I’ve missed something obvious. Looking forward to learning from the community and thanks in advance for any help.