Skip to main content
Associate
April 30, 2024
Solved

Configuring UART on STM32F103C8T6 (Bluepill) kills connection to ST-Link

  • April 30, 2024
  • 3 replies
  • 3986 views

When configuring UART on the board, according to https://wiki.st.com/stm32mcu/wiki/Getting_started_with_UART the program can be flashed once. When trying to flash again the system reports:

Target no device found

Error in initializing ST-LINK device.

Reason: No device found on target.

This happens even when just the configuration is set, no data transmitted and MS_USART_UARTx_Init() is commented out. The error occurs with every UART. It does not disappear when deleting the UART configuration in the IOC editor and regenerate the code without any references to UART. With BOOT0 set to high, reconnecting to ST-Link and flashing another program without configured UART the board behaves normally again. Commenting out HAL_Init() prevents this error, but I strongly assume that leads to other problems. This only happens to the Bluepill board, testing the same configuration with an STM32F407VGT6 (STM32F4-Discovery and an STM32F401CEU6 (Blackpill) stay inconspicuously.

Any ideas how to circumvent this behavior?

This topic has been closed for replies.
Best answer by Andrew Neil

@waclawek.jan wrote:

it's unlikely that you have an STM32 on a bluepill board.


Indeed.

@hbr  See this thread for a current example of the tale of woe resulting from the bluepill fakery:

https://community.st.com/t5/stm32-mcus-products/blue-pill-stm32f1-board-gets-programmed-through-arduino-ide-but/td-p/667923

3 replies

waclawek.jan
Super User
April 30, 2024

Make sure your program does not set AFIO_MAPR.SWJ_CFG in a way which disables debugging.

Also make sure you don't set system clock outside its operational envelope.

Also, it's unlikely that you have an STM32 on a bluepill board.

JW

Andrew Neil
Andrew NeilBest answer
Super User
April 30, 2024

@waclawek.jan wrote:

it's unlikely that you have an STM32 on a bluepill board.


Indeed.

@hbr  See this thread for a current example of the tale of woe resulting from the bluepill fakery:

https://community.st.com/t5/stm32-mcus-products/blue-pill-stm32f1-board-gets-programmed-through-arduino-ide-but/td-p/667923

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
hbrAuthor
Associate
May 1, 2024

Thanks for the link. I made some further investigations with other tools and it strongly looks like I got a clone. In my reply to @waclawek.jan I gave some more details.

The clones are getting better, my ST-Link V2 has a clone inside, an APM32F103CBT6. STLinkUpgrade v3.15.6 updated the firmware without complains.

This was the first project where some trouble occurred, so I didn't think it could be a fake.

MNapi
Senior II
April 30, 2024

How do you have pins PA14, PA13 setup ?

Debug -> No Debug  (then the problem is here)

or

Debug -> Serial Wire

 

1.png

 

2.png

hbrAuthor
Associate
May 1, 2024

Thanks for Your answer. The problem seems to be another one. It is very unlikely that I used a real ST MCU but a fake one. This was the first topic I run into trouble with the clone.

Peter BENSCH
Technical Moderator
April 25, 2025

This thread relates to a so-called Blue Pill, which uses illegally cloned STM32F103. ST resources are only dedicated to supporting genuine ST products. We are not committed to ensuring that clones/fakes products work properly with the firmware we provide.

We recommend to purchase genuine products from STMicroelectronics and purchase them from known and trusted distributors.

This thread will now be locked. However, if you face difficulties while using genuine ST products, we’re here to assist you. Please feel free to start a new thread, and our team, along with community members, will be ready to help you with any issues/questions you encounter.

Thank you for your understanding.

Regards
/Peter