CubeProgrammer + Clone STLinkV2 Full chip erase fails; OK in CubeIDE
Title edited to note that this is a clone ST-Link.
Using a WeAct mini STM32H723 Core board which seems to be working fine via SWD and a gold STLInkV2 USB stick. (STLinkV2 firmware V2j46S7).
Using STM32CubeProgrammer v2.21.0 seems to work ok, connected under SWD, 4kHz, Normal mode, S/w reset, reliable speed, non shared (my usual settings that work with all the other STM32 boards I have).
But when I tried the "Full chip erase" (or erase selected sectors), it merely reports erase successful with no errors. However the flash remains unchanged.
Using STM32CubeIDE 2.0.0 however, I can successfully download my code to the board (which proves the flash can be erased using the STLinkV2 h/w).
Not sure where the problem lies as yet, but have put this issue up here in case others have the same problem with STM32CubeProgrammer.
Will post an update here or on the WeAct github site if I make progress to finding why its not working.