Skip to main content
WGao.1
Associate II
May 28, 2021
Solved

Does STUSB4500 support DR_Swap Message?

  • May 28, 2021
  • 1 reply
  • 1289 views

Hello,

When I connect USB-C source power to our device, PD sniffer shows Source:DFP sends DR_Swap message to our device, which has a STUSB4500 PD controller. However, our device(Sink:UDP) always sends Reject command.

My questions are:

  • Does STUSB4500 support DR_Swap message?
  • We want to swap data role based on PD negotiation, how to get the message and how to process it to reply Accept?
  • Is there a register that record the DR_Swap message?
  • From STUSB4500, is there a way to trigger to have PD source to send the DR_Swap message again?

Thanks,

Winston

    This topic has been closed for replies.
    Best answer by Gregory Go.

    Hello,

    No the STUSB4500 doesn't support the DataRole_Swap message.

    The STUSB4500 role is a Power Sink. And following the USB PD specification, a Power Sink always start as UFP (Device).

    If you want to change the default role, you need indeed to send a PowerRole_Swap or DataRole_swap command. But these commands are not supported by STUSB4500.

    To send DR_Swap command, you need to use a USB PD solution which implement this optional command, like:

    - STM32F0 + STUSB1602

    - or STM32G0 + TCPP01

    1 reply

    Gregory Go.
    Gregory Go.Best answer
    Senior III
    June 3, 2021

    Hello,

    No the STUSB4500 doesn't support the DataRole_Swap message.

    The STUSB4500 role is a Power Sink. And following the USB PD specification, a Power Sink always start as UFP (Device).

    If you want to change the default role, you need indeed to send a PowerRole_Swap or DataRole_swap command. But these commands are not supported by STUSB4500.

    To send DR_Swap command, you need to use a USB PD solution which implement this optional command, like:

    - STM32F0 + STUSB1602

    - or STM32G0 + TCPP01