Skip to main content
NWins.1
Visitor II
January 5, 2021
Solved

EMIF06-MSD02N16 Level 4 IEC ESD Typo?

  • January 5, 2021
  • 2 replies
  • 800 views

Hello, reading about the EMIF06-MSD02N16 datasheet it's quoting that it complies with IEC ESD 61000-4-2 Level 4 however the air discharge voltages quoted are 12kV. IEC 61000-4-2 specifies the air discharge Level 4 voltage as 15kV. Is this a typo, as the datasheet quotes 8kV Contact (which is correct for Level 4 IEC ESD)

This topic has been closed for replies.
Best answer by FGUIT

Hello,

Updated datasheet is on st.com (https://www.st.com/resource/en/datasheet/emif06-msd02n16.pdf), with +/-15kV air discharge on pins connected to SDcard socket.

Best regards.

2 replies

FGUIT
ST Employee
January 11, 2021

Hello,

You're right, this is a typo, EMIF06-mSD02N16 withstands 15kV air discharge IEC 61000-4-2. Datasheet is under modification and will be updated on st.com.

Best regards.

FGUIT
FGUITBest answer
ST Employee
January 21, 2021

Hello,

Updated datasheet is on st.com (https://www.st.com/resource/en/datasheet/emif06-msd02n16.pdf), with +/-15kV air discharge on pins connected to SDcard socket.

Best regards.