ESD and Transient protection circuit- ISO 7637-3 and ISO 10605
- March 12, 2025
- 1 reply
- 767 views
Hello ST team,
We are currently developing and ECU for tractor. The ECU have many Digital inout and outputs to interface with sensors and other subsytems of the tractor. For the GPIO we have identified the ESDALY device suitable, since it conforms to the ISO standards for ESD and transients ISO 7637-3 and ISO 10605. We are planning to use ESDA5V3LY for our digital input and output circuits in the ECU as the operational voltage is 5V. Based on that we have designed the circuit for DI and DO and we did LTSpice simulation of the circuit too and found that results seems ok. Kindly help us in finalising the circuits before proceeding with PCB design, as there are very minimal reference circuits available. The circuits are attached for reference. Please reply.