Skip to main content
Associate
July 18, 2025
Question

EVSPIN32F0601S1 not running motor

  • July 18, 2025
  • 0 replies
  • 156 views

Hi All,

I am trying to get up and running the above hardware. I downloaded the software for the board, and we already use IAR compiler here. After compiling and downloading (via the STLink), the system runs the program just fine.

However, I just need to run the system with the onboard POT and it is not moving or energizing the motor at all.

I changed the 6step_conf.h file to POTENTIOMETER_INTERFACE = 1 and all others to 0. Nothing happens.

All the voltages to the board are perfect (running 70VDC to the board via a 7 amp programmable power supply).

All help would be greatly appreciated. This is my first intro into using the part. Time is very tight.

regards,
Charles