Skip to main content
Visitor II
July 7, 2023
Question

Flash Default Firmware STA8100_D0

  • July 7, 2023
  • 0 replies
  • 1195 views

I am using the GNSS receiver STA8100GA and the EVAL board EVB-TAPP_E1. 

Yesterday I wanted to change the protocol from RTCM to NMEA. To do this I used the FW configuration window to set RTCM_OB_OFF_SWITCH = 0 & RTCM3_ON_OFF_SWITCH = 0 and NMEA_OVER_UART_ON_OFF to 1 and NMEA_UART_PORT_NUMBER to port0.

After applying the new configuration and reconnecting the device, Teseo Suite can't detect my receiver.

The receiver is also not detected when I add it manually with all possible configurations. 

So I think I've done something wrong.  

Is there a way to flash the default firmware without Teseo Suite (because I can't find the device in the FW configuration panel)? 

This topic has been closed for replies.