Skip to main content
Gerd G
Visitor II
February 9, 2018
Question

Have a wifi problem with STSW-3DP001_-_3D_printer_board

  • February 9, 2018
  • 3 replies
  • 1052 views
Posted on February 09, 2018 at 21:06

Board boot ok

WiFi connect Pc or Tablat ok (192.168.0.2)

ping 192.168.0.1 ok

https://community.st.com/external-link.jspa?url=http%3A%2F%2F192.168.0.1%2Fcommand.shtml

load ok

click to button (Send the command) G-conde command line M115 --> no action and no Platform respond

or

https://community.st.com/external-link.jspa?url=http%3A%2F%2F192.168.0.1%2Ffilemgt.shtml

load ok

G code file monagment

click to button (Get G codes file list) --> no action and no Platform respond

or

3D printer configuration file

click to button (Get config) --> no action and no Platform respond

--> nothing happens

--> wifi connection error

ping 192.168.0.1 --> Destination Host Unreachable

--- I do

sw4stm32_linux_64bits-v2.4 - install

Firmware download en.stsw3dp001.zip

Project import in 'System Workbench for STM32'

Build Project ok

Marlin.bin --> Board flash ok

Debug Project no problems visible - no error

Board boot ok

click to button

--> nothing happens

--> wifi connection error

Can you help me, what can I do.

Is the board faulty?

#wifi #stsw-3dp001 #3d-printer-board
    This topic has been closed for replies.

    3 replies

    Senior III
    February 12, 2018
    Posted on February 12, 2018 at 11:45

    Hi !

    First your post appears as 'assumed answered', why ?

    On topic, I have the same board, and if I'm correct, the web server is handled entirely by the wifi chip, and it will communicate only what is needed to the F401, which handles all the hardware side. Also I think that you need an SD card with some specific files on it (this is a marlin stuff). Again I am not really sure...

    I must say that the support for this board is not top notch, at least on this forum. Maybe if you ask directly ST you can have a better answer...

    Anh Vu
    Associate
    June 7, 2018
    Posted on June 07, 2018 at 12:16

    i got totally the same problem with you ! did you solved it ? i cant change the name ssid and the password of wifi also. so i think problem is communication from wifi module and st chip. but still cant fix yet. if you have the solution. please put it here or send me an email at :

    mailto:chimchichclick@gmail.com

     ! thanks !
    Anh Vu
    Associate
    June 8, 2018
    Posted on June 08, 2018 at 07:47

    i using IAR ide and problem is solved. so, i dont know  where is problem with SW4STM32 IDE