Skip to main content
GOetj
Visitor II
May 22, 2019
Question

HDMI ESD(?) IC Identification

  • May 22, 2019
  • 3 replies
  • 2525 views

Hello! I am trying to identify an IC that is connected to an Xbox One X's HDMI 2.1 output.

The markings on the chip appear as:

(ST logo)

NFD (1st Line)

741 (2nd Line)

There are 18 solder balls attached to the pcb from the chip, arranged as so (after removing the chip):

0690X000008wDMCQA2.jpg

From what I have searched so far, it appears that the chip is most likely an IC acting as an HDMI esd filter, but I cannot find a chip with the same pin layout.

It would be really appreciated if someone could assist me in sourcing this chip.

Thank you!

This topic has been closed for replies.

3 replies

RKazi.1
Visitor II
July 10, 2020

I would like an answer to the same question. This is definitely a IC chip that should be available to purchase instead of being forced to salvage from donor motherboards. Please provide an option for purchasing this IC chip.

RKazi.1
Visitor II
July 20, 2020

GOetj, I just pulled this chip off of a broken Xbox one X board and took a picture of the back side of it under my microscope. Not that it will help with replacing it, but I figured you'd like to see what it looks like. STMicroelectronics, Please make this IC available to purchase! I would be willing to buy a decent amount of them to resale if you can make a run of them.

0693W000001tF1XQAU.jpg

Visitor II
August 19, 2023

Here is an alternative:

Xbox Series X / S / Xbox One X ESD Booster IC Alternative. 

https://www.ubermicro.co.uk/product/xbox-esd-hdmi-booster-u21-alternative-for-series-x-series-s-and-one-x/