Skip to main content
Rohit Thomas
Visitor II
July 26, 2019
Question

Help in designing a 600V to 24V, 3A isolated DC-DC converter

  • July 26, 2019
  • 0 replies
  • 1015 views

I have designed an isolated AC-DC converter, 300 to 590V AC input (400V AC nom) to 24V, 4A output using the L6566-BH Controller in eDesignSuite. Attaching the details herewith.

Any further guidance regarding the Design implementation in actual Hardware ?

I would also like to actually design for multiple outputs for the same input: - 1) 24V, 3A 2) 5V, 3A

I was not able to design this using the tool, I'm guessing it's a limitation of the tool. Would like some help in this regard also.

This topic has been closed for replies.