Skip to main content
Dave Kearney
Associate II
October 4, 2020
Question

Hi, could you confirm that the EMIF06-HSD03F3 footprint has bga pads that are all 0.4mm from each other? The datasheet drawing of the footprint is a bit misleading and has the pads asymmetrical, but it looks like from the dimensions that it is symetr

  • October 4, 2020
  • 4 replies
  • 1250 views
This topic has been closed for replies.

4 replies

Mohamed S.
ST Employee
October 6, 2020

Hello Dave,

I confirm that EMIF06-HSD03F3 has bump pads that are all 0.4mm from each other as shown in figure 12 of its datasheet and reproduced below.

I hope this answers your question.

Do not hesitate to look at our resources like ESD FAQ or ESD protections for MCUs peripherals to make sure your design is robust against any ESD surge that can enter from any connector exposed to ESD discharge.

0693W000004IoFrQAK.png

Dave Kearney
Associate II
October 6, 2020

Thanks, do you think it would make sense to redraw the above figure then? The pads are clearly not all the same distance apart on the drawing - the middle column of pads is noticeably closer to the right than the left on both drawings in the datasheet - so it is a bit confusing.

Cheers,

Dave

DSass.1
Visitor II
January 17, 2023

Just to make sure : Bump side = bottom side?

Thanks

Dori

Mohamed S.
ST Employee
January 18, 2023

Yes, bump side is bottom side.