Skip to main content
DRech.1
Visitor II
May 4, 2020
Question

Hi, L6387ED is used in STM's B-G431B-ESC1 which uses 3.3V logic when the L6387ED is only rated for 3.6V minimum high level logic threshold. Can L6387ED be reliably used at 3.3V? Please see additional details below.

  • May 4, 2020
  • 0 replies
  • 740 views

The L6387ED datasheet indicates that the high level logic threshold is 3.6V as a minimum.

 https://www.st.com/resource/en/datasheet/l6387e.pdf#page=7

The STM ESC eval kit (P/N: B-G431B-ESC1) definitely uses the L6387ED. We checked schematics and a some physical samples.

https://www.st.com/resource/en/schematic_pack/mb1419-g431cb-b01_schematic.pdf#page=4

However, the STM32G4 in the B-G431B-ESC1 only supplies 3.3V logic to the L6387ED.

We would like to use L6387ED in our product but only if it’s actually rated for 3.3V logic.

This topic has been closed for replies.