Skip to main content
Sabou
Associate
March 5, 2019
Question

How to send AT commands to the integrated wifi-module using internal uart in B-L475E-IOT1A

  • March 5, 2019
  • 4 replies
  • 1574 views

I want to communicate with the wifi module integrated in the STM32 iot node using AT commands, so i configure the internal uart3 used by the module to receive AT commands and transmit the answer to the AT command but it doesn't work ?

    This topic has been closed for replies.

    4 replies

    Mike_ST
    Technical Moderator
    March 5, 2019

    Well, I guess that according to the example in the CubeMX package, even though the board is UART capable, the ISM43362-M3G-L44 on this board has the SPI only firmware.

    https://www.inventeksys.com/iwin/firmware/

    Sabou
    SabouAuthor
    Associate
    March 5, 2019

    yes i try with the spi firmware and it works ; But the goal of my project is not to use the firmware , i need to establish a simple and basic communication with the integrated wifi-module using AT commands through the internal uart or spi (uart3 or spi3 used by the wifi module ) , is that possible ?

    Mike_ST
    Technical Moderator
    March 5, 2019

    Yes AT commands over SPI3 will work, not over UART3.

    Sabou
    SabouAuthor
    Associate
    March 7, 2019

    yes, i've tried to send AT commands over SPI and it works ,i followed the IWIN guide for AT commands But still have a problem in two AT commands:C1=SSID and C2=Password to join a network, and I want to know if there is a special way or format to send this two commands ?