Associate
September 1, 2022
Question
I need hardware error feedback. Or also possible improvements in the design.
- September 1, 2022
- 1 reply
- 1942 views
I'm using the theseo-liv3f module to make a GNSS board. In this project, I am only acquiring invalid positioning data, and I would like to know if there are any hardware errors to be corrected. I've already paid attention to the reset pin which is actibe low, and making corrections, I managed to update the firmware, but the data is still invalid.
I'm using the active antenna Taoglass AGGBP.SLS.25A