Skip to main content
SVora.4
Visitor II
February 5, 2019
Question

I2C setting is not working for FP-ATR-LORA1 package (GNSS + LoRa asset tracker)

  • February 5, 2019
  • 1 reply
  • 725 views

To reproduce

  • Enable I2C in gnss_app_cfg.h
#define configUSE_I2C 1
  • When moved, the UART log said

(11:58:08.056) -->�?�Going�?�to�?�run...

(11:58:12.943) Can�?�not�?�read�?�axes

(11:58:12.963) >>�?�sensor_event

(11:58:15.875) Accelerometer�?�NOT�?�initialized

Everything is ok for default UART setting. One possible issue is the configuration of I2C1 in interrupt mode for Teseo component with background reading.

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    March 13, 2019

    Hi

    In the FP-ATR-LORA1 the GNSS is not supported on I2C bus.

    It's a design decision because GNSS (in Geofencing mode) is used to wakeup the whole system (from standby) sending a message via UART.

    This can not be done on I2C.

    Hope this helps

    Regards

    Francesco