Skip to main content
Visitor II
February 3, 2025
Solved

Identify this component - LIS344ALH?

  • February 3, 2025
  • 2 replies
  • 1086 views

Hi,

 

Are you able to identify the below products from their product markings?  I believe they should both be the LIS344ALH but one of them is behaving strangely. The 34AH marked product is reading 1g (2.332V) in the z axis when placed flat on a desk. The ones with markings 34AL are reading 0.7g (2.117V) when in the same position. I have switched the ICs around to rule out a PCB fault, but the difference always follows the IC, suggesting there is a difference between the AL and AH marking. I can't find any details on the datasheet outlining product markings to understand the codes printed on top of the IC.

 

 A057 - 20250203_115100.bmpA055 - 20250203_111204.bmp

 

Thanks

 

Matt

Best answer by Peter BENSCH

Welcome @Matt_UK, to the community!

I am extremely sorry to have to inform you that the LIS344xx accelerometers have long been discontinued and that STMicroelectronics no longer has any information about them. As sensor markings are/were also still internal information, you will probably not find any information in the vastness of the otherwise never-forgetting internet.

I am very sorry not to be able to give you more pleasant information.

Regards
/Peter

2 replies

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
February 3, 2025

Welcome @Matt_UK, to the community!

I am extremely sorry to have to inform you that the LIS344xx accelerometers have long been discontinued and that STMicroelectronics no longer has any information about them. As sensor markings are/were also still internal information, you will probably not find any information in the vastness of the otherwise never-forgetting internet.

I am very sorry not to be able to give you more pleasant information.

Regards
/Peter

AScha.3
Super User
February 3, 2025

The chips from rs also have  AH marking:

AScha3_0-1738591630317.png

So just replace the chips with wrong marking.

"If you feel a post has answered your question, please click ""Accept as Solution""."