Skip to main content
CGrov.1
Associate III
February 1, 2021
Question

Imported project file errors

  • February 1, 2021
  • 2 replies
  • 1302 views

I am importing a project that a colleague made. The project seems to be missing a lot of include files, I know I have the correct libraries in my repository but the project can't seem to find them. It seems like the filepath is pointing to C:/users/colleague/STM32Cube....

but I need to change it to C:/users/myUsername/STM32Cube....

Some of the CDT build console errors:

compilation terminated.
make[1]: *** [Middlewares/CMSIS/CMSIS/DSP/Source/TransformFunctions/subdir.mk:115: Middlewares/CMSIS/CMSIS/DSP/Source/TransformFunctions/arm_bitreversal.o] Error 1
make[1]: *** Waiting for unfinished jobs....
../Middlewares/CMSIS/CMSIS/DSP/Source/TransformFunctions/arm_cfft_f32.c:30:10: fatal error: arm_common_tables.h: No such file or directory
 #include "arm_common_tables.h"
 ^~~~~~~~~~~~~~~~~~~~~
compilation terminated.
../Middlewares/CMSIS/CMSIS/DSP/Source/TransformFunctions/arm_cfft_radix2_init_f32.c:30:10: fatal error: arm_common_tables.h: No such file or directory
 #include "arm_common_tables.h"
 ^~~~~~~~~~~~~~~~~~~~~
../Middlewares/CMSIS/CMSIS/DSP/Source/TransformFunctions/arm_cfft_radix2_init_q31.c:30:10: fatal error: arm_common_tables.h: No such file or directory
 #include "arm_common_tables.h"
 ^~~~~~~~~~~~~~~~~~~~~
compilation terminated.
compilation terminated.

This is a screenshot from my project explorer:

0693W000007DQ9wQAG.png 

How do I resolve include issues like this?

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
February 1, 2021

The joy of bad tools..

Probably should consider putting shared projects and repositories in a common directory both can access.

The project file is likely XML/ASCII open in a text editor and search/replace \user\blokeone\ for \user\bloketwo\

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
CGrov.1
CGrov.1Author
Associate III
February 1, 2021

Ok that seems to have eliminated most of the errors. I'm getting a new one now though:

0693W000007DSSvQAO.pngThe filepath is addressing the right user now (me). I think this new error is caused by using a different compiler than the one originally used by the project creator. I tried cleaning and building but no luck.

CGrov.1
CGrov.1Author
Associate III
February 1, 2021

I got past this error by changing to an internal builder

Project->properties->C/C# builder-> builder settings.

Now dealing with an issue of the IDE not generating a .elf file.