Skip to main content
IGent.1
Visitor II
December 13, 2019
Question

Is the MOSFET (STP85NF55L) reliability affected if the Vgs is near to the maximum specified in the datasheet?

  • December 13, 2019
  • 0 replies
  • 491 views

My customer specifies a relation of 60% of the maximum Vgs for operation. My design is using 80% of the maximum Vgs. They are asking how this increase will affect the component reliability (failure mechanism, failure rate...).

My design is eqquiped with 4 STP85NF55L, operating at 32Hz (PWM) resistive loads.

This topic has been closed for replies.