Skip to main content
JSong.4
Visitor II
September 8, 2022
Solved

L200CH and L200CV _ Power and Current Regulator

  • September 8, 2022
  • 1 reply
  • 1084 views

Can some one be so kind to let me know the difference between those 2 regulators?

Is it bending angel of the pin or the SPQ?

Thanks

This topic has been closed for replies.
Best answer by Peter BENSCH

Welcome, @JSong.4​, to the community!

L200 has been discontinued for a long time, but the following assignment applied:

  • L200CH: Pentawatt package, horizontal mounting, i.e. component resting on PCB and parallel to it, 90° angled THT pins
  • L200CV: Pentawatt package, vertical mounting, i.e. component standing on PCB straight THT pins
  • L200T, L200CT: TO-3 package

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards,

/Peter

1 reply

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
September 9, 2022

Welcome, @JSong.4​, to the community!

L200 has been discontinued for a long time, but the following assignment applied:

  • L200CH: Pentawatt package, horizontal mounting, i.e. component resting on PCB and parallel to it, 90° angled THT pins
  • L200CV: Pentawatt package, vertical mounting, i.e. component standing on PCB straight THT pins
  • L200T, L200CT: TO-3 package

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards,

/Peter