Looking for a substitute for the following part STTH512(DPAK) to a SOD132 (DO-123) package.
..
..
So the question is not about an alternative in a smaller enclosure, but about general alternatives due to the current worldwide shortage of components: unfortunately, there is no alternative in the same or compatible package in this power class, only the STTH812 could come into question, but it is only available in larger packages like the thru-hole TO-220AC or the D2PAK. Of course, there are also other devices with an even higher current capability and therefore a much larger package.
Good luck!
If the problem is resolved or answered, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.