Skip to main content
Visitor II
August 21, 2025
Solved

PLC module with ADC and mcu

  • August 21, 2025
  • 1 reply
  • 842 views

Could you please suggest a PLC module that includes a signal scaling unit and an isolation circuit, equipped with a high-speed sampling ADC with up to 16-bit resolution? The module should also integrate a microcontroller featuring SPI, LAN (Ethernet), SD card storage, and an HDMI port.”

Best answer by Peter BENSCH

Welcome @rakesh1184, to the community!

What do you mean by PLC – Power Line Communication or a Programmable Logic Controller?

In both cases, however, STMicroelectronics does not offer ready-made modules. For these, you will need to contact the relevant manufacturers.

Regards
/Peter

1 reply

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
August 21, 2025

Welcome @rakesh1184, to the community!

What do you mean by PLC – Power Line Communication or a Programmable Logic Controller?

In both cases, however, STMicroelectronics does not offer ready-made modules. For these, you will need to contact the relevant manufacturers.

Regards
/Peter