Skip to main content
Associate
November 28, 2023
Solved

Power MOSFETS in case of fast charging using BMS

  • November 28, 2023
  • 2 replies
  • 1638 views

I am working on building a BMS using L9961 IC, based on a research I figured out that in case of fast charging it is suggested to add two or more power MOSFET gates in parallel as seen in the figure below to reduce temperature rise and ensure reliable operation of the power MOSFET. Is there any draw backs for the following configuration ?

Best Regards,

Mohamed Smaili

Mohamed_Smaili_0-1701156367533.png

 

This topic has been closed for replies.
Best answer by Peter BENSCH

Welcome @Mohamed_Smaili, to the community!

CHG and DCHG have limited drive currents (data sheet, table 25, IPD = max 85mA), which limits the maximum gate capacitance to be driven (CPRDRV_LOAD = typ. 10nF). If you want to connect MOSFETs in parallel and do not want to use additional gate drivers, please pay particular attention to the exact same type of the MOSFETs at CHG and DCHG, and also to very low gate capacitance of these MOSFETs.

Hope that helps?

Regards
/Peter

2 replies

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
November 28, 2023

Welcome @Mohamed_Smaili, to the community!

CHG and DCHG have limited drive currents (data sheet, table 25, IPD = max 85mA), which limits the maximum gate capacitance to be driven (CPRDRV_LOAD = typ. 10nF). If you want to connect MOSFETs in parallel and do not want to use additional gate drivers, please pay particular attention to the exact same type of the MOSFETs at CHG and DCHG, and also to very low gate capacitance of these MOSFETs.

Hope that helps?

Regards
/Peter

Associate
November 29, 2023

Thanks @Peter BENSCH very beneficial.

Have a nice day!

Best Regards,

Mohamed Smaili