Associate II
March 22, 2024
Solved
Request for Device (IMS T225-F20E) Tolerance Data for Crystal Aging Analysis
- March 22, 2024
- 1 reply
- 1400 views
Hi
In our design, we incorporated the IMS T225-F20E component. This part necessitates a clock with a frequency of 5 MHz. According to note 3 in the attached image, crystal oscillators with a 200 ppm (parts per million) tolerance can be employed. However, this information pertains to scenarios where two devices are connected together by a link.
Now, the question is: What is the allowable tolerance for the clock oscillator if only one device is used?”
I am currently working on crystal aging analysis. It would be beneficial if you could furnish the allowable tolerance data for the device.


Thanks in advance