Skip to main content
Visitor II
June 28, 2023
Question

SM6T39CAY is not compliant for ISO 7637-2 Pulse 5a and 5b

  • June 28, 2023
  • 0 replies
  • 910 views

The below mentioned parts are failing for the ISO 7637-2 Pulse 5a and 5b. I have attached the image of the simulation result which we have done for the ISO 7637-2 pulse 5a in that the maximum power is went beyond the rated power of SM6T39CAY TVS diode(SM6T39CAY).

1.) SM6T39CAY

We need the suggestion from the STM Microelectronics for the alternate TVS diode which need to be compliant for the below mentioned ISO 7637-2 standard. The ISO 7637-2 Pulse 5a and Pulse 5b is our critical requirement. The below mentioned standards are our design requirements.

  1. Pulse 1
  2. Pulse 2
  3. Pulse 3a and Pulse 3b
  4. Pulse 4
  5. Pulse 5a and 5b

madhanprasathtta_0-1687937335548.png

 

This topic has been closed for replies.