Skip to main content
ScottT
Associate
January 3, 2019
Question

SPWF04S MiniAP mode issues

  • January 3, 2019
  • 3 replies
  • 1042 views

I've recently updated some SPWF04SA modules to firmware version 1.1.0 and I have a couple of problems with Mini AP mode:

  • The SSID I set with AT+S.SSIDTXT=<SSID> seems to be being truncated to 6 characters in the beacon frame, even though the WIND:26 notification gives the full SSID. I don't remember seeing this problem with firmware version 1.0.0. I've even tried setting wifi_ssid_len explicitly to the correct size, but it makes no difference.

  • If I configure for WPA2 security (wifi_priv_mode=2), it still appears as an unsecured AP, and I can connect to it without a password. The full message sequence is as follows:

+WIND:1:Poweron:171117-0328fe3-SPWF04S

+WIND:13:Copyright (c) 2012-2017 STMicroelectronics, Inc. All rights Reserved:SPWF04SA

+WIND:0:Console active

+WIND:3:Watchdog Running:20

AT+S.WIFI=0

AT-S.ERROR:18:Radio not running

AT+S.SCFG=wifi_tx_power,0

AT-S.OK

AT+S.SCFG=ip_use_httpd,0

AT-S.OK

AT+S.SCFG=ip_use_tftpd,0

AT-S.OK

AT+S.SCFG=ip_use_v6,0

AT-S.OK

AT+S.SCFG=ip_ntp_startup,0

AT-S.OK

AT+S.WIFI=0

AT-S.ERROR:18:Radio not running

AT+S.SSIDTXT=<my SSSID>

AT-S.OK

AT+S.SCFG=wifi_wpa_psk_text,<my password>

AT-S.OK

AT+S.SCFG=wifi_auth_type,0

AT-S.OK

AT+S.SCFG=wifi_priv_mode,2

AT-S.OK

AT+S.SCFG=wifi_mode,3

AT-S.OK

AT+S.WIFI=1

AT-S.OK

+WIND:32:WiFi Hardware Started

+WIND:26:Started AP:<my SSSID>

+WIND:24:WiFi Up:0:192.168.0.50

AT+S.GCFG=ip_netmask

AT-S.Var:ip_netmask=255.255.255.0

AT-S.OK

+WIND:28:Station Associated:00:0F:00:4F:B1:3F:0

[...]

Am I missing something somewhere?

Thanks in advance,

Scott.

    This topic has been closed for replies.

    3 replies

    Elio Cometti
    Visitor II
    January 7, 2019

    ​Hello Scott,

    the command sequence seems correct.

    I don't see the WIND:46: WPA Crunching PSK: indication, that may confirm the MiniAP is starting in open mode.

    I also checked the truncated SSID, but I cannot reproduce it on my side.

    I kindly ask you to restore the factory setting:

    AT+S.FCFG

    AT+S.WCFG

    AT+S.RESET

    then wait for "WIND:32: WiFi Hardware Started" and then send your sequence above (AT+S.WIFI=0, ...).

    Best Regards,

    Elio

    ScottT
    ScottTAuthor
    Associate
    January 9, 2019

    Thanks for your reply, Elio. After much experimentation, the following sequence of commands seems to start MiniAP mode with WPA2 enabled (and the full un-truncated SSID) consistently. I had to reset the module after the AT+S.WCFG using the reset pin instead of AT+S.RESET as it seemed to stop responding to commands when I used that.

    +WIND:1:Poweron:171117-0328fe3-SPWF04S

    +WIND:13:Copyright (c) 2012-2017 STMicroelectronics, Inc. All rights Reserved:SPWF04SA

    +WIND:0:Console active

    +WIND:3:Watchdog Running:20

    AT+S.WIFI=0

    AT-S.ERROR:18:Radio not running

    +WIND:32:WiFi Hardware Started

    AT+S.SCFG=wifi_mode,3

    AT-S.OK

    AT+S.WCFG

    AT-S.OK

    +WIND:1:Poweron:171117-0328fe3-SPWF04S

    +WIND:13:Copyright (c) 2012-2017 STMicroelectronics, Inc. All rights Reserved:SPWF04SA

    +WIND:0:Console active

    +WIND:3:Watchdog Running:20

    +WIND:32:WiFi Hardware Started

    AT+S.WIFI=0

    AT-S.OK

    +WIND:26:Started AP:<my SSID>

    +WIND:49:WPA Terminated:0

    +WIND:38:WiFi Powered Down

    AT+S.SCFG=wifi_tx_power,0

    AT-S.OK

    AT+S.SCFG=ip_use_httpd,0

    AT-S.OK

    AT+S.SCFG=ip_use_tftpd,0

    AT-S.OK

    AT+S.SCFG=ip_use_v6,0

    AT-S.OK

    AT+S.SCFG=ip_ntp_startup,0

    AT-S.OK

    AT+S.WIFI=0

    AT-S.ERROR:18:Radio not running

    AT+S.SSIDTXT=<my SSID>

    AT-S.OK

    AT+S.SCFG=wifi_wpa_psk_text,<my password>

    AT-S.OK

    AT+S.SCFG=wifi_auth_type,0

    AT-S.OK

    AT+S.SCFG=wifi_priv_mode,2

    AT-S.OK

    AT+S.SCFG=wifi_mode,3

    AT-S.OK

    AT+S.WIFI=1

    AT-S.OK

    +WIND:46:WPA Crunching PSK:<my password>:14

    +WIND:32:WiFi Hardware Started

    +WIND:26:Started AP:<my SSID>

    +WIND:24:WiFi Up:0:192.168.0.50

    Waiting for the WIND 32 after reset, before issuing AT+S.WIFI=0 seems to be crucial, as does resetting after setting and saving wifi_mode so that it is set to the desired value at boot time. Also I think AT+S.WIFI=0 needs to be sent before wifi_mode is set before the reset.

    I have also observed a further issue with MiniAP mode - the DHCP server will by default offer to clients a default gateway address of 165.165.165.165. Surely this is erroneous?

    Elio Cometti
    Visitor II
    January 9, 2019

    ​Hi Scott,

    at boot the WiFi Hardware will be started or not depending on the hardware state at last AT+S.WCFG command.

    Actually:

    • the AT+S.WCFG command was issued when the WiFi Hardware was started: at next boot you should wait for WIND:32: and issue the AT+S.WIFI=0 command if you wish to change any wifi_* config variable;
    • the AT+S.WCFG command was issued when the WiFi Hardware was stopped: at next boot you have to wait WIND:0:, as the WIND:32: will never come;

    At this point you can change any wifi_* config variable.

    The observation about default gateway address may give interoperability problem with some devices, upgrading to a newer FW is recommended for this (please contact your ST dealer for getting the FW package).

    Regards,

    Elio